<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic qn9080 flash memory for user in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/qn9080-flash-memory-for-user/m-p/1421487#M12928</link>
    <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;We are going to use the flash memory of QN9080 to store the product serial number.&lt;BR /&gt;The size to be used is within 100 bytes.&lt;/P&gt;&lt;P&gt;(1) Is it okay to use QN's flash for user purposes?&lt;BR /&gt;(2) Which memory address is allowed for user purposes? (ex 0x3107 0000 ? )&lt;BR /&gt;&lt;BR /&gt;-----------------more info&lt;/P&gt;&lt;P&gt;I think I found a function suitable for reading and writing internal ROM memory.&lt;BR /&gt;- framework / Flash / External / Source / Eeprom_InternalFlash.c&lt;BR /&gt;- EEPROM_ReadData(), EEPROM_WriteData()&lt;/P&gt;&lt;P&gt;When tested with this function, the data is stored and read well.&lt;BR /&gt;Is it okay to read and write data to the internal ROM memory using this function?&lt;/P&gt;&lt;P&gt;Reards,&lt;/P&gt;&lt;P&gt;Jung-jin&lt;/P&gt;</description>
    <pubDate>Sun, 06 Mar 2022 02:34:37 GMT</pubDate>
    <dc:creator>jung-jin</dc:creator>
    <dc:date>2022-03-06T02:34:37Z</dc:date>
    <item>
      <title>qn9080 flash memory for user</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/qn9080-flash-memory-for-user/m-p/1421487#M12928</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;We are going to use the flash memory of QN9080 to store the product serial number.&lt;BR /&gt;The size to be used is within 100 bytes.&lt;/P&gt;&lt;P&gt;(1) Is it okay to use QN's flash for user purposes?&lt;BR /&gt;(2) Which memory address is allowed for user purposes? (ex 0x3107 0000 ? )&lt;BR /&gt;&lt;BR /&gt;-----------------more info&lt;/P&gt;&lt;P&gt;I think I found a function suitable for reading and writing internal ROM memory.&lt;BR /&gt;- framework / Flash / External / Source / Eeprom_InternalFlash.c&lt;BR /&gt;- EEPROM_ReadData(), EEPROM_WriteData()&lt;/P&gt;&lt;P&gt;When tested with this function, the data is stored and read well.&lt;BR /&gt;Is it okay to read and write data to the internal ROM memory using this function?&lt;/P&gt;&lt;P&gt;Reards,&lt;/P&gt;&lt;P&gt;Jung-jin&lt;/P&gt;</description>
      <pubDate>Sun, 06 Mar 2022 02:34:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/qn9080-flash-memory-for-user/m-p/1421487#M12928</guid>
      <dc:creator>jung-jin</dc:creator>
      <dc:date>2022-03-06T02:34:37Z</dc:date>
    </item>
  </channel>
</rss>