<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックpn5180 icode inquiry</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/pn5180-icode-inquiry/m-p/1382255#M12508</link>
    <description>&lt;P&gt;Hi NXP&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now we develloping a product with a PN5180 and NfcrdlibEX5_ISO15693_MCUX&amp;nbsp; library&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can we tag a I-code NFC on that project?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you !&lt;/P&gt;</description>
    <pubDate>Tue, 07 Dec 2021 01:54:24 GMT</pubDate>
    <dc:creator>lim</dc:creator>
    <dc:date>2021-12-07T01:54:24Z</dc:date>
    <item>
      <title>pn5180 icode inquiry</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/pn5180-icode-inquiry/m-p/1382255#M12508</link>
      <description>&lt;P&gt;Hi NXP&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now we develloping a product with a PN5180 and NfcrdlibEX5_ISO15693_MCUX&amp;nbsp; library&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can we tag a I-code NFC on that project?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you !&lt;/P&gt;</description>
      <pubDate>Tue, 07 Dec 2021 01:54:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/pn5180-icode-inquiry/m-p/1382255#M12508</guid>
      <dc:creator>lim</dc:creator>
      <dc:date>2021-12-07T01:54:24Z</dc:date>
    </item>
    <item>
      <title>Re: pn5180 icode inquiry</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/pn5180-icode-inquiry/m-p/1383023#M12516</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Please kindly find the detail information as the below:&lt;/P&gt;
&lt;P&gt;Example 5 - ISO15693&lt;BR /&gt;Similar to the previous example, this one is also using only one technology, in that case ISO15693. “DiscoveryLoop” is configured to resolve only one device and in the example it is shown how to change Tx Guard Time for T5T cards, this is implemented in “phApp_Init()” function.&lt;BR /&gt;Once ICODE SLI is resolved and activated, application printout card information like type of the card and UID, and it will read and write from/to the memory block.&lt;BR /&gt;This example is good start in case of working with only one card or to see how to manage ISO15693 type of the cards.&lt;BR /&gt;For a much more extensive example, demonstrating the use of ISO/IEC 15693 and ISE/IEC 18000-3 Mode 3 tags (ICODE SLI and ICODE ILT). In order to assure ICODE SLI and ILT detection please check HAL digital delay define settings as described in chapter 4.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Dec 2021 02:49:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/pn5180-icode-inquiry/m-p/1383023#M12516</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-12-08T02:49:05Z</dc:date>
    </item>
    <item>
      <title>Re: pn5180 icode inquiry</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/pn5180-icode-inquiry/m-p/1383225#M12520</link>
      <description>&lt;P&gt;Thank you for replying me&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you have any idea about icode-1&lt;/P&gt;&lt;P&gt;does that project support icode-1?&lt;/P&gt;&lt;P&gt;so if support icode-1 ,can i get a example library source please?&lt;/P&gt;</description>
      <pubDate>Wed, 08 Dec 2021 07:57:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/pn5180-icode-inquiry/m-p/1383225#M12520</guid>
      <dc:creator>lim</dc:creator>
      <dc:date>2021-12-08T07:57:26Z</dc:date>
    </item>
    <item>
      <title>Re: pn5180 icode inquiry</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/pn5180-icode-inquiry/m-p/1383232#M12521</link>
      <description>&lt;P&gt;Thank you for replying me&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you have any idea about icode-1(one)&lt;/P&gt;&lt;P&gt;does that project support icode-1(one)?&lt;/P&gt;&lt;P&gt;so if support icode-1(one) ,can i get a example library source please?&lt;/P&gt;</description>
      <pubDate>Wed, 08 Dec 2021 08:04:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/pn5180-icode-inquiry/m-p/1383232#M12521</guid>
      <dc:creator>lim</dc:creator>
      <dc:date>2021-12-08T08:04:22Z</dc:date>
    </item>
    <item>
      <title>Re: pn5180 icode inquiry</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/pn5180-icode-inquiry/m-p/1383683#M12529</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Would you please provide what does mean for the&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;icode-1?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There is no the part number in&amp;nbsp; NXP website.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;URL:&amp;nbsp;&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/icode:MC_42024" target="_blank"&gt;https://www.nxp.com/products/rfid-nfc/nfc-hf/icode:MC_42024&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 09 Dec 2021 02:42:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/pn5180-icode-inquiry/m-p/1383683#M12529</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-12-09T02:42:28Z</dc:date>
    </item>
  </channel>
</rss>