<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックFRDM-KW 36 CAN Module issue</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW-36-CAN-Module-issue/m-p/1372734#M12403</link>
    <description>&lt;P&gt;In FRDM-KW 36 board I downloaded the SDK file from example projects(CAN loop back example code).I run the above example on MCU XPRESSO IDE, while debugging I am unable to read the data on CAN Pins(it means in CAN_H ,CAN_L &amp;amp; Transmit ,receive pins).&lt;/P&gt;</description>
    <pubDate>Wed, 17 Nov 2021 11:56:10 GMT</pubDate>
    <dc:creator>vardhan</dc:creator>
    <dc:date>2021-11-17T11:56:10Z</dc:date>
    <item>
      <title>FRDM-KW 36 CAN Module issue</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW-36-CAN-Module-issue/m-p/1372734#M12403</link>
      <description>&lt;P&gt;In FRDM-KW 36 board I downloaded the SDK file from example projects(CAN loop back example code).I run the above example on MCU XPRESSO IDE, while debugging I am unable to read the data on CAN Pins(it means in CAN_H ,CAN_L &amp;amp; Transmit ,receive pins).&lt;/P&gt;</description>
      <pubDate>Wed, 17 Nov 2021 11:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW-36-CAN-Module-issue/m-p/1372734#M12403</guid>
      <dc:creator>vardhan</dc:creator>
      <dc:date>2021-11-17T11:56:10Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KW 36 CAN Module issue</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW-36-CAN-Module-issue/m-p/1372920#M12407</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. In the readme.txt of the example you can see that "the example will send a CAN Message from the Tx Message Buffer to the Rx Message Buffer throuth &lt;U&gt;internal&lt;/U&gt; loopback interconnect". The example shows how to use the loopback test mode to debug the CAN Bus design.&lt;/P&gt;
&lt;P&gt;Can you check the flexcan_interrupt_transfer example? In this example, 2 boards are connected through CAN bus. You can find the Board settings in the readme.txt. And don't forget the 12V power supply on J32.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Wed, 17 Nov 2021 18:52:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW-36-CAN-Module-issue/m-p/1372920#M12407</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2021-11-17T18:52:01Z</dc:date>
    </item>
  </channel>
</rss>