<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: Not given options in Protocol Analzer Adapter window</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Not-given-options-in-Protocol-Analzer-Adapter-window/m-p/1358739#M12235</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192544"&gt;@shellpry2&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The USB that you have supports Bluetooth LE using the examples that we provide, You could use the device as a master or slave depending on your application.&lt;/P&gt;
&lt;P&gt;But the device doesn't support the sniffer protocol because it is not enabled as a promiscuous mode for the Bluetooth LE protocol.&lt;/P&gt;
&lt;P&gt;What is the issue that you are facing on? Are you trying to connect to a different device?&lt;/P&gt;
&lt;P&gt;Regads,&lt;/P&gt;
&lt;P&gt;Mario&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 20 Oct 2021 14:55:52 GMT</pubDate>
    <dc:creator>mario_castaneda</dc:creator>
    <dc:date>2021-10-20T14:55:52Z</dc:date>
    <item>
      <title>Not given options in Protocol Analzer Adapter window</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Not-given-options-in-Protocol-Analzer-Adapter-window/m-p/1357251#M12198</link>
      <description>&lt;P&gt;I'm trying to grab a BLE connection and follow it through adv to disconnect. I'm using a demo code set. The device is displaying correctly in the IoT Toolbox app on my phone too. I'm using a NXP sniffer and the Protocol Analyzer.&lt;/P&gt;&lt;P&gt;My issue is that I'm not given BLE options or an options other than to click on the channel. The analyzer sees my sniffer (Com6 JN5189/K32W) and connects through to my wireshark via the local area connection. But nothing is showing on the wireshark capture. If I use different sniffer, I'm able to see traffic. But I can't seem to get anything going with the NXP Protocol Analyzer and sniffer.&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;</description>
      <pubDate>Mon, 18 Oct 2021 14:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Not-given-options-in-Protocol-Analzer-Adapter-window/m-p/1357251#M12198</guid>
      <dc:creator>shellpry2</dc:creator>
      <dc:date>2021-10-18T14:17:08Z</dc:date>
    </item>
    <item>
      <title>Re: Not given options in Protocol Analzer Adapter window</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Not-given-options-in-Protocol-Analzer-Adapter-window/m-p/1358089#M12218</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192544"&gt;@shellpry2&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I looked at the image that you shared. Unfortunately, that device doesn't support the BLE Sniffer.&lt;/P&gt;
&lt;P&gt;I could recommend the USB KW41/KW36 or KW38 &lt;A href="https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/USB-KW41-Bluetooth-LE-Sniffer-Application-Update/ta-p/1100565" target="_self"&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;USB-KW41 Bluetooth LE Sniffer Application Update&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;The JN5189 and K32W are recommended for the 802.15.4 communication.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;Mario&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Oct 2021 20:04:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Not-given-options-in-Protocol-Analzer-Adapter-window/m-p/1358089#M12218</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2021-10-19T20:04:13Z</dc:date>
    </item>
    <item>
      <title>Re: Not given options in Protocol Analzer Adapter window</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Not-given-options-in-Protocol-Analzer-Adapter-window/m-p/1358634#M12233</link>
      <description>&lt;P&gt;The usb dongle and the K32W I'm using both came from the IOTZTB-DK006. It specifically calls out Zigbee, Thread, and BLE as being usable.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/wireless/multiprotocol-mcus/advanced-development-kit-for-k32w061-and-jn5189-88:IOTZTB-DK006" target="_blank"&gt;https://www.nxp.com/products/wireless/multiprotocol-mcus/advanced-development-kit-for-k32w061-and-jn5189-88:IOTZTB-DK006&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/wireless/multiprotocol-mcus/k32w-usb-dongle-for-bluetooth-le-zigbee-and-thread-networks:OM15080-K32W" target="_self"&gt;https://www.nxp.com/products/wireless/multiprotocol-mcus/k32w-usb-dongle-for-bluetooth-le-zigbee-and-thread-networks:OM15080-K32W&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The dongle in the kit is listed as the OM15080-K32W for BLE, Zigbee, and Thread. But it sounds like you are saying it doesn't support BLE? Did I read that correctly?&lt;/P&gt;</description>
      <pubDate>Wed, 20 Oct 2021 12:27:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Not-given-options-in-Protocol-Analzer-Adapter-window/m-p/1358634#M12233</guid>
      <dc:creator>shellpry2</dc:creator>
      <dc:date>2021-10-20T12:27:26Z</dc:date>
    </item>
    <item>
      <title>Re: Not given options in Protocol Analzer Adapter window</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Not-given-options-in-Protocol-Analzer-Adapter-window/m-p/1358739#M12235</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192544"&gt;@shellpry2&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The USB that you have supports Bluetooth LE using the examples that we provide, You could use the device as a master or slave depending on your application.&lt;/P&gt;
&lt;P&gt;But the device doesn't support the sniffer protocol because it is not enabled as a promiscuous mode for the Bluetooth LE protocol.&lt;/P&gt;
&lt;P&gt;What is the issue that you are facing on? Are you trying to connect to a different device?&lt;/P&gt;
&lt;P&gt;Regads,&lt;/P&gt;
&lt;P&gt;Mario&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Oct 2021 14:55:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Not-given-options-in-Protocol-Analzer-Adapter-window/m-p/1358739#M12235</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2021-10-20T14:55:52Z</dc:date>
    </item>
    <item>
      <title>Re: Not given options in Protocol Analzer Adapter window</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Not-given-options-in-Protocol-Analzer-Adapter-window/m-p/1358742#M12236</link>
      <description>&lt;P&gt;I was just looking to sniff a connection between the K32W and my mobile device. Looks like I need to get a sniffer. Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 20 Oct 2021 14:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Not-given-options-in-Protocol-Analzer-Adapter-window/m-p/1358742#M12236</guid>
      <dc:creator>shellpry2</dc:creator>
      <dc:date>2021-10-20T14:58:57Z</dc:date>
    </item>
  </channel>
</rss>