<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックJN5189THN: internal EEPROM API manual or examples</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/JN5189THN-internal-EEPROM-API-manual-or-examples/m-p/1354515#M12170</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;How can I find the API of internal EEPROM usage or example codes for JN5189THN?&lt;/P&gt;&lt;P&gt;I tried to look over header files in SDK2_6_3 or 4, however I could not find such kind of definitions.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 13 Oct 2021 01:56:00 GMT</pubDate>
    <dc:creator>usaygo</dc:creator>
    <dc:date>2021-10-13T01:56:00Z</dc:date>
    <item>
      <title>JN5189THN: internal EEPROM API manual or examples</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189THN-internal-EEPROM-API-manual-or-examples/m-p/1354515#M12170</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;How can I find the API of internal EEPROM usage or example codes for JN5189THN?&lt;/P&gt;&lt;P&gt;I tried to look over header files in SDK2_6_3 or 4, however I could not find such kind of definitions.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Oct 2021 01:56:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189THN-internal-EEPROM-API-manual-or-examples/m-p/1354515#M12170</guid>
      <dc:creator>usaygo</dc:creator>
      <dc:date>2021-10-13T01:56:00Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189THN: internal EEPROM API manual or examples</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189THN-internal-EEPROM-API-manual-or-examples/m-p/1354552#M12171</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Please check the co-ordinator example.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="nxf56274_0-1634092690921.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/158937iE624CB9AD813CB02/image-size/medium?v=v2&amp;amp;px=400" role="button" title="nxf56274_0-1634092690921.png" alt="nxf56274_0-1634092690921.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;nxf56274_0-1634092690921.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Oct 2021 02:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189THN-internal-EEPROM-API-manual-or-examples/m-p/1354552#M12171</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-10-13T02:38:24Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189THN: internal EEPROM API manual or examples</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189THN-internal-EEPROM-API-manual-or-examples/m-p/1354817#M12173</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thank for the quick response.&lt;/P&gt;&lt;P&gt;The coordinator's code is using internal flash as EEPROM emulation.&lt;/P&gt;&lt;P&gt;I totally misunderstood about internal EEPROM, which I thought the EEPROM was direct function of MCU.&amp;nbsp;Correctly the EEPROM is connected through I2C2 bus.&lt;/P&gt;&lt;P&gt;Now I could managed to control Flash and NTAG's I2C2 EEPROM. Thanks!&lt;/P&gt;&lt;P&gt;Information pointer:&lt;/P&gt;&lt;P&gt;internal flash: easy to find information in `fsl_flash.[ch]'.&lt;BR /&gt;NTAG eeprom: From NTAG example, the file `i2c_jn_fsl.[ch]' is low level access for reading,writing data to EEPROM. The ntag_driver.[ch] provide higher level of read/write of eeprom and register access.&lt;BR /&gt;By seeing the code from `ntag_i2c_plus', these files are not considered about C++. (#if defined __cplusplus extern "C" ...). Hope to add this issue into the problem management.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 13 Oct 2021 08:59:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189THN-internal-EEPROM-API-manual-or-examples/m-p/1354817#M12173</guid>
      <dc:creator>usaygo</dc:creator>
      <dc:date>2021-10-13T08:59:28Z</dc:date>
    </item>
  </channel>
</rss>