<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: NFC RF active error flag</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/NFC-RF-active-error-flag/m-p/1354200#M12168</link>
    <description>&lt;P&gt;Ok the status could be read from RX_STATUS register. I realized that after RF_ON command I am stuck on STATE_CHANGE_IRQ_STAT (I am waiting for TX_RFON_IRQ_STAT). In this moment I can see sinus vawes on oscilloscope. If I ignore it I will be stuck waiting for the RX_STATUS register to reflect the TRANSCEIVE_STATE. If I ignore both, the TX_RFON_IRQ_STAT appears after few SEND_DATA sequences. Is there any state diagram that could help me to diagnose the problem? For example which state may IRQ_STATUS register reflect after RF_ON command and so on? Any help is appreciated.&lt;/P&gt;</description>
    <pubDate>Tue, 12 Oct 2021 10:55:32 GMT</pubDate>
    <dc:creator>Leeenka</dc:creator>
    <dc:date>2021-10-12T10:55:32Z</dc:date>
    <item>
      <title>NFC RF active error flag</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NFC-RF-active-error-flag/m-p/1353957#M12167</link>
      <description>&lt;P&gt;Dear developers,&lt;/P&gt;&lt;P&gt;we have the PN5180 connected to Raspberry Pi. I have followed instructions from here &lt;A href="https://www.nxp.com/docs/en/application-note/AN12650.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12650.pdf&lt;/A&gt; for the ISO/IEC 14443 - REQA. After I sent REQA command I repeatedly read IRQ_STATUS register to check the status and RX_STATUS to check number of bytes received. The number of received bytes are 0 and in the IRQ status reported bits are 1:2:4:5:10 and after I place a card also bit 0. What does mean that RF active error IRQ status? We also have not the BUSY pin connected. Could it also cause wrong behavior?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Oct 2021 06:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NFC-RF-active-error-flag/m-p/1353957#M12167</guid>
      <dc:creator>Leeenka</dc:creator>
      <dc:date>2021-10-12T06:49:25Z</dc:date>
    </item>
    <item>
      <title>Re: NFC RF active error flag</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NFC-RF-active-error-flag/m-p/1354200#M12168</link>
      <description>&lt;P&gt;Ok the status could be read from RX_STATUS register. I realized that after RF_ON command I am stuck on STATE_CHANGE_IRQ_STAT (I am waiting for TX_RFON_IRQ_STAT). In this moment I can see sinus vawes on oscilloscope. If I ignore it I will be stuck waiting for the RX_STATUS register to reflect the TRANSCEIVE_STATE. If I ignore both, the TX_RFON_IRQ_STAT appears after few SEND_DATA sequences. Is there any state diagram that could help me to diagnose the problem? For example which state may IRQ_STATUS register reflect after RF_ON command and so on? Any help is appreciated.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Oct 2021 10:55:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NFC-RF-active-error-flag/m-p/1354200#M12168</guid>
      <dc:creator>Leeenka</dc:creator>
      <dc:date>2021-10-12T10:55:32Z</dc:date>
    </item>
    <item>
      <title>Re: NFC RF active error flag</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NFC-RF-active-error-flag/m-p/1360241#M12246</link>
      <description>&lt;P&gt;Hello LEEENKA,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in using our PN5180 bard for your design. Have you explored the possibility of using the board with our &lt;A href="https://www.nxp.com/design/designs/nfc-reader-library-software-support-for-nfc-frontend-solutions:NFC-READER-LIBRARY" target="_self"&gt;NFC Reader Library&lt;/A&gt;? There is a well-explained Application Note for guiding you on how&amp;nbsp;to install NXP’s NFC Reader Library on a GNU/Linux system (&lt;A href="https://www.nxp.com/docs/en/application-note/AN11802.pdf" target="_self"&gt;AN11802&lt;/A&gt;).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Oct 2021 18:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NFC-RF-active-error-flag/m-p/1360241#M12246</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2021-10-22T18:36:40Z</dc:date>
    </item>
  </channel>
</rss>