<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic QN9080: unable to program the device. in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/QN9080-unable-to-program-the-device/m-p/1345124#M12083</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In our company we have designed 2 boards that are both using the&amp;nbsp;QN9080-001-M17AZ Bluetooth Module. We have followed the design rules and we are making use of the SWDIO, SWCLK, RESETN and ISP pins with the correct configuration in terms of pins and pull-up/pull-down resistors. However, in neither of these boards are we able to successfully connect to the QN9080 and program it. The MCU_Xpresso is giving an error that the device is not discoverable.&amp;nbsp;&lt;BR /&gt;Is there something we did not take into account? According to the datasheets, there is not anything wrong. Any help is appreciated &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;Vasilis&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 23 Sep 2021 14:16:56 GMT</pubDate>
    <dc:creator>Vasilis</dc:creator>
    <dc:date>2021-09-23T14:16:56Z</dc:date>
    <item>
      <title>QN9080: unable to program the device.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9080-unable-to-program-the-device/m-p/1345124#M12083</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In our company we have designed 2 boards that are both using the&amp;nbsp;QN9080-001-M17AZ Bluetooth Module. We have followed the design rules and we are making use of the SWDIO, SWCLK, RESETN and ISP pins with the correct configuration in terms of pins and pull-up/pull-down resistors. However, in neither of these boards are we able to successfully connect to the QN9080 and program it. The MCU_Xpresso is giving an error that the device is not discoverable.&amp;nbsp;&lt;BR /&gt;Is there something we did not take into account? According to the datasheets, there is not anything wrong. Any help is appreciated &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;Vasilis&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 14:16:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9080-unable-to-program-the-device/m-p/1345124#M12083</guid>
      <dc:creator>Vasilis</dc:creator>
      <dc:date>2021-09-23T14:16:56Z</dc:date>
    </item>
    <item>
      <title>Re: QN9080: unable to program the device.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9080-unable-to-program-the-device/m-p/1346163#M12091</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;What is your programmer? Jlink? Check the module's voltage and XTAL. Is the voltage 3.3V? Does the crystal work normally?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Sun, 26 Sep 2021 01:33:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9080-unable-to-program-the-device/m-p/1346163#M12091</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-09-26T01:33:16Z</dc:date>
    </item>
    <item>
      <title>Re: QN9080: unable to program the device.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9080-unable-to-program-the-device/m-p/1346270#M12093</link>
      <description>&lt;P&gt;We are using the PEMicro debugging interface. We eventually found 2 issues on some of our boards:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Some pins were not soldered correctly, probably to wrong mask used by the PCB manufacturer.&lt;/LI&gt;&lt;LI&gt;The RESETN port should not be connected to the debugger, since it is controlled by the SWDIO port as well.&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Sun, 26 Sep 2021 08:52:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9080-unable-to-program-the-device/m-p/1346270#M12093</guid>
      <dc:creator>Vasilis</dc:creator>
      <dc:date>2021-09-26T08:52:48Z</dc:date>
    </item>
  </channel>
</rss>