<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: NFC Keyless</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/NFC-Keyless/m-p/1330650#M11854</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The reading distance of the application. For the NFC tag. Only ICODE can up to 1.5m. But it depends on the antenna.&lt;BR /&gt;we do not have a reader in our portfolio that meets your requirements.&lt;BR /&gt;Nonetheless, you can check it as the link.&lt;BR /&gt;URL:&lt;A href="https://www.nxp.com/products/rfid-nfc/rfid-ecosystem:RFID_ECOSYSTEMS" target="_blank"&gt;https://www.nxp.com/products/rfid-nfc/rfid-ecosystem:RFID_ECOSYSTEMS&lt;/A&gt;&lt;BR /&gt;A selection of different reader manufacturers, solution providers and systems integrators around the world, I'm almost sure that you can find a reader that meets your requirements with one of the available ones in the list.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you! &lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Fri, 27 Aug 2021 01:32:47 GMT</pubDate>
    <dc:creator>fangfang</dc:creator>
    <dc:date>2021-08-27T01:32:47Z</dc:date>
    <item>
      <title>NFC Keyless</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NFC-Keyless/m-p/1330238#M11849</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Is NFC the solution&lt;BR /&gt;I have a “receiver” that cannot have a larger antenna than approx 30x50 x 10 mm on the PCB.&lt;BR /&gt;It may be possible to have a wire wound coil size 140x79 mm. The PCB will then be “inside” the coil.&lt;BR /&gt;The receiver has “unlimited” 12V power supply.&lt;BR /&gt;The transmitter is a remote control you have in your pocket. It has no buttons.&lt;BR /&gt;It is supplied from a battery CR2450. Battery life shall be at least one year.&lt;BR /&gt;An accelerometer turns on the transmitter during a time when motion is detected.&lt;BR /&gt;Transmitter will at maximum be on 10h / working day.&lt;BR /&gt;Using bidirectional communication this may be replaced by a “receiver” making a wake up on the “transmitter”&lt;BR /&gt;The receiver shall read an unique key code from the transmitter (4 bytes, battery status bit and checksum) when it is approx 1 meter or closer from the receiver&lt;BR /&gt;At 10m or longer it must not detect the transmitter&lt;BR /&gt;Best regards&lt;BR /&gt;Göran Nilsson&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 09:20:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NFC-Keyless/m-p/1330238#M11849</guid>
      <dc:creator>gorannilsson</dc:creator>
      <dc:date>2021-08-26T09:20:42Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Keyless</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NFC-Keyless/m-p/1330650#M11854</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The reading distance of the application. For the NFC tag. Only ICODE can up to 1.5m. But it depends on the antenna.&lt;BR /&gt;we do not have a reader in our portfolio that meets your requirements.&lt;BR /&gt;Nonetheless, you can check it as the link.&lt;BR /&gt;URL:&lt;A href="https://www.nxp.com/products/rfid-nfc/rfid-ecosystem:RFID_ECOSYSTEMS" target="_blank"&gt;https://www.nxp.com/products/rfid-nfc/rfid-ecosystem:RFID_ECOSYSTEMS&lt;/A&gt;&lt;BR /&gt;A selection of different reader manufacturers, solution providers and systems integrators around the world, I'm almost sure that you can find a reader that meets your requirements with one of the available ones in the list.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you! &lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 27 Aug 2021 01:32:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NFC-Keyless/m-p/1330650#M11854</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-08-27T01:32:47Z</dc:date>
    </item>
  </channel>
</rss>