<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38 in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1325116#M11737</link>
    <description>&lt;P&gt;How do you update the firmware? Do you hold the reset button, and then plug in? Does the disk show something like 'daplinkboot'? Then drag the 'sniffer_usbkw38_k22f_0x8000.bin' into it.&lt;/P&gt;</description>
    <pubDate>Wed, 18 Aug 2021 03:16:25 GMT</pubDate>
    <dc:creator>nxf56274</dc:creator>
    <dc:date>2021-08-18T03:16:25Z</dc:date>
    <item>
      <title>Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1324001#M11671</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;could you please check and confirm that USB-KW38 BLE sniffing works using current program versions?&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Win 10 Pro - version 2004&lt;/LI&gt;&lt;LI&gt;Virtual Com Port (COM3) installed&lt;/LI&gt;&lt;LI&gt;USB-KW-38 + k22f_bl_07132016.bin&lt;/LI&gt;&lt;LI&gt;Kinetis Protocol Analyzer Adapter 2.0.4.1&lt;/LI&gt;&lt;LI&gt;tap-windows-9.24.2-I601-Win10&lt;/LI&gt;&lt;LI&gt;WinPcap 4.1.3&lt;/LI&gt;&lt;LI&gt;USBPcap 1.5.4.0&lt;/LI&gt;&lt;LI&gt;Wireshark-win64-3.4.7&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Kinetis Protocol Analyzer shown no BLE interface available.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 16 Aug 2021 16:39:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1324001#M11671</guid>
      <dc:creator>SHotmar</dc:creator>
      <dc:date>2021-08-16T16:39:10Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1324264#M11690</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I test the 2.0.4.1. It works fine. Do you close the firewall?&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 03:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1324264#M11690</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-08-17T03:19:10Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1324652#M11720</link>
      <description>&lt;P&gt;The firewall has no impact.&lt;/P&gt;&lt;P&gt;KPAA shows in Settings&amp;gt; Default Virtual interface: Virtual Interface Off. And it is the only choice.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I feel the&amp;nbsp;C:\NXP\Kinetis Protocol Analyzer Adapter 2.0.4.1\USB-KW Dongle Drivers\fsl_ucwnt.inf driver is not compatible with KPAA. KPAA can't find any virtual interface.&lt;/P&gt;&lt;P&gt;Could you please link me your driver?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 09:57:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1324652#M11720</guid>
      <dc:creator>SHotmar</dc:creator>
      <dc:date>2021-08-17T09:57:12Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1324851#M11725</link>
      <description>&lt;P&gt;Is there any way to check what's loaded inside USB-KW38?&lt;/P&gt;&lt;P&gt;I even flashed the whole device with following bin files according to your manual.&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;usb-kw38z-OpenSDA.bin&lt;/LI&gt;&lt;LI&gt;sniffer_usbkw38_kw37z.bin&lt;/LI&gt;&lt;LI&gt;sniffer_usbkw38_k22f_0x8000.bin&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;And KPAA still tells me no sniffer detected:&lt;/P&gt;&lt;P&gt;C:\NXP\Kinetis Protocol Analyzer Adapter 2.0.4.1&amp;gt;KPAA_Cli.exe start -c COM3 -b all -i "Ethernet3"&lt;BR /&gt;Kinetis Protocol Analyzer Adapter version 2.0.4.1&lt;BR /&gt;Copyright (c) 2021 NXP. All rights reserved.&lt;BR /&gt;Autodetecting sniffers...&lt;BR /&gt;Please wait, this may take a while.&lt;BR /&gt;Error: No sniffer was detected.&lt;BR /&gt;Type exit to close the console app...&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 15:32:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1324851#M11725</guid>
      <dc:creator>SHotmar</dc:creator>
      <dc:date>2021-08-17T15:32:23Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1325116#M11737</link>
      <description>&lt;P&gt;How do you update the firmware? Do you hold the reset button, and then plug in? Does the disk show something like 'daplinkboot'? Then drag the 'sniffer_usbkw38_k22f_0x8000.bin' into it.&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 03:16:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1325116#M11737</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-08-18T03:16:25Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1325314#M11762</link>
      <description>&lt;P&gt;I do it according to your manual: Getting Started with the USB-KW38 &amp;gt; 2.4 Programming USB-KW38 as Sniffer &amp;gt;&amp;nbsp;USING BOOTLOADER MODE QSG -&amp;nbsp;&lt;A href="https://www.nxp.com/document/guide/getting-started-with-the-usb-kw38:GS-USB-KW38#title1.1" target="_blank"&gt;https://www.nxp.com/document/guide/getting-started-with-the-usb-kw38:GS-USB-KW38#title1.1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;So, I do:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;get to DAPLINKBOOT&lt;/LI&gt;&lt;LI&gt;put&amp;nbsp;usb-kw38z-OpenSDA.bin to DAPLINKBOOT, unplug and plug&lt;/LI&gt;&lt;LI&gt;put sniffer_usbkw38_kw37z.bin to USB-KW37Z, unplug&lt;/LI&gt;&lt;LI&gt;get to DAPLINKBOOT&lt;/LI&gt;&lt;LI&gt;put&amp;nbsp;sniffer_usbkw38_k22f_0x8000.bin to DAPLINKBOOT, unplug and plug&lt;/LI&gt;&lt;LI&gt;... and sniffer should be programmed and running...&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Is it right?&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 08:23:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1325314#M11762</guid>
      <dc:creator>SHotmar</dc:creator>
      <dc:date>2021-08-18T08:23:19Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1325343#M11765</link>
      <description>&lt;P&gt;You are right. So the KPPA still can't recognize the sniffer? How many usb-kw38 do you have? Do all of them bad?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 08:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1325343#M11765</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-08-18T08:56:55Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1325356#M11766</link>
      <description>&lt;P&gt;I have only one USB-KW38 right now. What can go wrong if I am able to program a device?&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 09:17:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1325356#M11766</guid>
      <dc:creator>SHotmar</dc:creator>
      <dc:date>2021-08-18T09:17:33Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1326536#M11773</link>
      <description>&lt;P&gt;You only have one device. So we can't find out which is the reason, the device or the software.&lt;/P&gt;
&lt;P&gt;And if you want to sniffer the ble packet, you need three usb-kw to detect three avd channel separately.&lt;/P&gt;
&lt;P&gt;Now, You can download the other ble program like 'w_uart' for usb-kw to check if the ble can work well.&lt;/P&gt;</description>
      <pubDate>Fri, 20 Aug 2021 01:37:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1326536#M11773</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-08-20T01:37:31Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1327807#M11800</link>
      <description>&lt;P&gt;I've just tested the second USB-KW38. It behaves exactly the same as the first one. No sniffer detected in Kinetis Protocol Analyzer Adapter 2.0.4.1.&lt;/P&gt;&lt;P&gt;Both my USB-KW38 are REV A1. Date Code: 9D2015 Registration date: 02.06.2021 and 21.07.2021.&lt;/P&gt;&lt;P&gt;So, there is a great probability the hardware is working properly. It has to be a software issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please provide me older version of&amp;nbsp;&amp;nbsp;Kinetis Protocol Analyzer Adapter. Thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 23 Aug 2021 13:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1327807#M11800</guid>
      <dc:creator>SHotmar</dc:creator>
      <dc:date>2021-08-23T13:07:20Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1328184#M11810</link>
      <description>&lt;P&gt;Did you try the software on other's PC? I do not find the old version. The attachment is not the install package. It copied from my computer. Put it in directory 'c:/nxp'.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Aug 2021 03:52:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1328184#M11810</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-08-24T03:52:10Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Protocol Analyzer Adapter 2.0.4.1 + USB-KW38</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1330488#M11853</link>
      <description>&lt;P&gt;Heureka. Kinetis Protocol Analyzer Adapter 2.0.&lt;STRONG&gt;2&lt;/STRONG&gt;.1&amp;nbsp;works with USB-KW38 in latest Windows 10.&lt;/P&gt;&lt;P&gt;I had to use Wireshark 3.2.16 (older version) too because Wireshark 3.4.8 contains wrong btle_ex.dll compiled for Wireshark 3.2.x only.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, I have to inform you that something is wrong with&amp;nbsp;Kinetis Protocol Analyzer Adapter 2.0.&lt;STRONG&gt;4&lt;/STRONG&gt;.1 and it doesn't find USB-KW38 in Windows 10.&lt;/P&gt;&lt;P&gt;Thank you for the older version.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 15:47:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Kinetis-Protocol-Analyzer-Adapter-2-0-4-1-USB-KW38/m-p/1330488#M11853</guid>
      <dc:creator>SHotmar</dc:creator>
      <dc:date>2021-08-26T15:47:49Z</dc:date>
    </item>
  </channel>
</rss>