<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックKW36 Temperature sensor sample code BLE disconnection problem</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/KW36-Temperature-sensor-sample-code-BLE-disconnection-problem/m-p/1321749#M11638</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When I used temp sensor sample code by kw36, I found that if I don't press button to transmit the temp from server to client, BLE would be disconnected by itself in a few seconds. Then I rewrite the code to make it transmit the temp every 500ms, but it still would be disconnected by itself.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How to make it remain connection status?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Wed, 11 Aug 2021 08:27:29 GMT</pubDate>
    <dc:creator>Lincoln</dc:creator>
    <dc:date>2021-08-11T08:27:29Z</dc:date>
    <item>
      <title>KW36 Temperature sensor sample code BLE disconnection problem</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW36-Temperature-sensor-sample-code-BLE-disconnection-problem/m-p/1321749#M11638</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When I used temp sensor sample code by kw36, I found that if I don't press button to transmit the temp from server to client, BLE would be disconnected by itself in a few seconds. Then I rewrite the code to make it transmit the temp every 500ms, but it still would be disconnected by itself.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How to make it remain connection status?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 11 Aug 2021 08:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW36-Temperature-sensor-sample-code-BLE-disconnection-problem/m-p/1321749#M11638</guid>
      <dc:creator>Lincoln</dc:creator>
      <dc:date>2021-08-11T08:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: KW36 Temperature sensor sample code BLE disconnection problem</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW36-Temperature-sensor-sample-code-BLE-disconnection-problem/m-p/1322101#M11640</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. Did you disable the Power Down functionality? This can be done in the app_preinclude.h (cPWR_UsePowerDownMode). With the Power Down mode enabled, if no key is pressed in an interval of 5 seconds, the sensor node disconnects and re-enters cPWR_DeepSleepMode&lt;/P&gt;
&lt;P&gt;For more information about the Temperature Sensor and Collector, I would recommend the "Bluetooth Low Energy Demo Applications User Guide.pdf" (Path: SDK_doc.zip\docs\wireless\Bluetooth).&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Wed, 11 Aug 2021 18:59:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW36-Temperature-sensor-sample-code-BLE-disconnection-problem/m-p/1322101#M11640</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2021-08-11T18:59:14Z</dc:date>
    </item>
  </channel>
</rss>