<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KW38A zephyr support in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/KW38A-zephyr-support/m-p/1318480#M11553</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Are there any plans to port zephyr for NXP KW38 (frdm-kw38) or any hints where to start from? How different is from KW41z to use it as a template (Are there any application similar to &lt;A href="https://www.nxp.com/docs/en/application-note/AN12560.pdf" target="_self"&gt;AN12560&lt;/A&gt;)?&lt;/P&gt;&lt;P&gt;Any hint is highly appreciated.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 04 Aug 2021 21:36:06 GMT</pubDate>
    <dc:creator>cezarburlacu</dc:creator>
    <dc:date>2021-08-04T21:36:06Z</dc:date>
    <item>
      <title>KW38A zephyr support</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW38A-zephyr-support/m-p/1318480#M11553</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Are there any plans to port zephyr for NXP KW38 (frdm-kw38) or any hints where to start from? How different is from KW41z to use it as a template (Are there any application similar to &lt;A href="https://www.nxp.com/docs/en/application-note/AN12560.pdf" target="_self"&gt;AN12560&lt;/A&gt;)?&lt;/P&gt;&lt;P&gt;Any hint is highly appreciated.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 04 Aug 2021 21:36:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW38A-zephyr-support/m-p/1318480#M11553</guid>
      <dc:creator>cezarburlacu</dc:creator>
      <dc:date>2021-08-04T21:36:06Z</dc:date>
    </item>
    <item>
      <title>Re: KW38A zephyr support</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW38A-zephyr-support/m-p/1318583#M11560</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We do not have the plan to port zephyr to kw38. The zephyr has the porting &lt;A href="https://docs.zephyrproject.org/latest/guides/porting/board_porting.html?highlight=porting" target="_self"&gt;guide&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;We do not have the doc to describe the difference between kw41 and kw38.&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 05 Aug 2021 01:51:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW38A-zephyr-support/m-p/1318583#M11560</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-08-05T01:51:57Z</dc:date>
    </item>
    <item>
      <title>Re: KW38A zephyr support</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW38A-zephyr-support/m-p/1319224#M11593</link>
      <description>&lt;P&gt;Thank you for your response. It is a pity that zephyr is not supported for this board; it would've been the single one with BLE and CAN on the same chip...&lt;/P&gt;</description>
      <pubDate>Thu, 05 Aug 2021 17:20:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW38A-zephyr-support/m-p/1319224#M11593</guid>
      <dc:creator>cezarburlacu</dc:creator>
      <dc:date>2021-08-05T17:20:10Z</dc:date>
    </item>
  </channel>
</rss>