<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: Couldn't run MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Couldn-t-run-MCUXpresso-IDE/m-p/1314609#M11449</link>
    <description>&lt;P&gt;Self-Answered&lt;/P&gt;&lt;P&gt;It needs JRE.&lt;/P&gt;</description>
    <pubDate>Wed, 28 Jul 2021 14:18:31 GMT</pubDate>
    <dc:creator>sChameleoNz</dc:creator>
    <dc:date>2021-07-28T14:18:31Z</dc:date>
    <item>
      <title>Couldn't run MCUXpresso IDE</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Couldn-t-run-MCUXpresso-IDE/m-p/1313995#M11444</link>
      <description>&lt;P&gt;I'm using MCUXpresso IDE v11.4.0.6224.&lt;/P&gt;&lt;P&gt;I installed SDK_2_6_3_JN5189DK6.&lt;/P&gt;&lt;P&gt;The tool works well in this point.&lt;/P&gt;&lt;P&gt;Next, I installed the Zigbee Configuration Editor plug-in.&lt;/P&gt;&lt;P&gt;And, I couldn't run the tool.&lt;/P&gt;&lt;P&gt;When I try to run the MCUXpresso IDE, the tool is automatically closed when it is opening.&lt;/P&gt;&lt;P&gt;I tried reinstall the tool after cleaning, 10 times, but it was the same every single time.&lt;/P&gt;&lt;P&gt;How do I use the MCUXpresso IDE with Zigbee Configuration Editor?&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jul 2021 15:14:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Couldn-t-run-MCUXpresso-IDE/m-p/1313995#M11444</guid>
      <dc:creator>sChameleoNz</dc:creator>
      <dc:date>2021-07-27T15:14:39Z</dc:date>
    </item>
    <item>
      <title>Re: Couldn't run MCUXpresso IDE</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Couldn-t-run-MCUXpresso-IDE/m-p/1314609#M11449</link>
      <description>&lt;P&gt;Self-Answered&lt;/P&gt;&lt;P&gt;It needs JRE.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jul 2021 14:18:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Couldn-t-run-MCUXpresso-IDE/m-p/1314609#M11449</guid>
      <dc:creator>sChameleoNz</dc:creator>
      <dc:date>2021-07-28T14:18:31Z</dc:date>
    </item>
  </channel>
</rss>