<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックkw32w041 not booting when GPIO5 is held low</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/kw32w041-not-booting-when-GPIO5-is-held-low/m-p/1293310#M11259</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am wondering whether there is anything the the NXP bootloader that prevents the&amp;nbsp;kw32w041 to boot up when I put low the GPIO5 before powering it up.&lt;/P&gt;&lt;P&gt;Any help is much appreciated.&lt;/P&gt;</description>
    <pubDate>Wed, 16 Jun 2021 13:40:20 GMT</pubDate>
    <dc:creator>jacinto1m</dc:creator>
    <dc:date>2021-06-16T13:40:20Z</dc:date>
    <item>
      <title>kw32w041 not booting when GPIO5 is held low</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/kw32w041-not-booting-when-GPIO5-is-held-low/m-p/1293310#M11259</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am wondering whether there is anything the the NXP bootloader that prevents the&amp;nbsp;kw32w041 to boot up when I put low the GPIO5 before powering it up.&lt;/P&gt;&lt;P&gt;Any help is much appreciated.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jun 2021 13:40:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/kw32w041-not-booting-when-GPIO5-is-held-low/m-p/1293310#M11259</guid>
      <dc:creator>jacinto1m</dc:creator>
      <dc:date>2021-06-16T13:40:20Z</dc:date>
    </item>
    <item>
      <title>Re: kw32w041 not booting when GPIO5 is held low</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/kw32w041-not-booting-when-GPIO5-is-held-low/m-p/1293452#M11261</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. The GPIO5 is also the ISP Entry pin:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Ricardo_Zamora_1-1623861987378.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147231i9E7E5D9E29683BFD/image-size/large?v=v2&amp;amp;px=999" role="button" title="Ricardo_Zamora_1-1623861987378.png" alt="Ricardo_Zamora_1-1623861987378.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;[3] ISP programming mode: leave pin floating high during reset to avoid entering UART programming mode or hold it low to program&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can find this information in the &lt;A href="https://www.nxp.com/docs/en/data-sheet/K32W041AM.pdf" target="_blank"&gt;Data Sheet&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jun 2021 16:47:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/kw32w041-not-booting-when-GPIO5-is-held-low/m-p/1293452#M11261</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2021-06-16T16:47:01Z</dc:date>
    </item>
  </channel>
</rss>