<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic QN908x Capacitive in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/QN908x-Capacitive/m-p/1261963#M11021</link>
    <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I would like to use Capacitive sensing on QN9080C MCU.&lt;BR /&gt;I already see AN12190, but this does not help (a lot of details related to source config/compile are missing into this AN).&lt;/P&gt;&lt;P&gt;I have some questions:&lt;/P&gt;&lt;P&gt;1. Is QN908x supported by touch library? Is yes, why touch library is not available in QN908x SDK (SDK_2.2.4_QN908XC for example)?&lt;/P&gt;&lt;P&gt;2. I got touch library because I download SDK_2.9.0_FRDM-KE15Z and I extract the library. I configure my project to include the library and I tried to compile, but I got some compilation error. For example, in "nt.h" file, I have this error:&lt;BR /&gt;&lt;BR /&gt;#if defined(CPU_QN908X) || defined(CPU_QN9080C)&lt;BR /&gt;#include "nt_module_cs.h"&lt;BR /&gt;#else&lt;BR /&gt;#include "nt_module_tsi.h"&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;Can not find "nt_module_cs.h" file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to search for a touch library example based on QN9080C, so I can get "nt_module_cs.h", but I have not success.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Conclusion:&lt;BR /&gt;do you think you will 100% support touch library into QN908x SDK? I expect to find touch library (code and working examples) into latest QN908x SDK.&lt;BR /&gt;&lt;BR /&gt;Thank you&lt;/P&gt;&lt;P&gt;Davide Ferrario&lt;/P&gt;</description>
    <pubDate>Wed, 14 Apr 2021 10:57:51 GMT</pubDate>
    <dc:creator>davideferrario</dc:creator>
    <dc:date>2021-04-14T10:57:51Z</dc:date>
    <item>
      <title>QN908x Capacitive</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN908x-Capacitive/m-p/1261963#M11021</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I would like to use Capacitive sensing on QN9080C MCU.&lt;BR /&gt;I already see AN12190, but this does not help (a lot of details related to source config/compile are missing into this AN).&lt;/P&gt;&lt;P&gt;I have some questions:&lt;/P&gt;&lt;P&gt;1. Is QN908x supported by touch library? Is yes, why touch library is not available in QN908x SDK (SDK_2.2.4_QN908XC for example)?&lt;/P&gt;&lt;P&gt;2. I got touch library because I download SDK_2.9.0_FRDM-KE15Z and I extract the library. I configure my project to include the library and I tried to compile, but I got some compilation error. For example, in "nt.h" file, I have this error:&lt;BR /&gt;&lt;BR /&gt;#if defined(CPU_QN908X) || defined(CPU_QN9080C)&lt;BR /&gt;#include "nt_module_cs.h"&lt;BR /&gt;#else&lt;BR /&gt;#include "nt_module_tsi.h"&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;Can not find "nt_module_cs.h" file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to search for a touch library example based on QN9080C, so I can get "nt_module_cs.h", but I have not success.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Conclusion:&lt;BR /&gt;do you think you will 100% support touch library into QN908x SDK? I expect to find touch library (code and working examples) into latest QN908x SDK.&lt;BR /&gt;&lt;BR /&gt;Thank you&lt;/P&gt;&lt;P&gt;Davide Ferrario&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 10:57:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN908x-Capacitive/m-p/1261963#M11021</guid>
      <dc:creator>davideferrario</dc:creator>
      <dc:date>2021-04-14T10:57:51Z</dc:date>
    </item>
    <item>
      <title>Re: QN908x Capacitive</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN908x-Capacitive/m-p/1265221#M11063</link>
      <description>&lt;P&gt;Hi Davide,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. As the &lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN12190.pdf" target="_blank"&gt;QN908x Capacitive Sensing Design Guide&lt;/A&gt; states, you should go to &lt;A href="https://www.nxp.com/design/sensor-developer-resources/touch-software:FREESCALE-TOUCH-SOFTWARE" target="_blank"&gt;NXP Touch Software Website&lt;/A&gt;, where you can find the related documentation about the Touch Software. And in the &lt;A href="https://mcuxpresso.nxp.com/en/select" target="_blank"&gt;SDK Builder&lt;/A&gt;, you can download the latest version of the library in the available platforms.&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 14:10:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN908x-Capacitive/m-p/1265221#M11063</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2021-04-20T14:10:56Z</dc:date>
    </item>
  </channel>
</rss>