<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic JN5189 send data in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-send-data/m-p/1258507#M10991</link>
    <description>Hi All, The chip I use is JN5189, and the SDK version I use is SDK2.6.2_JN5189. I developed based on the zigbee_coordinator,zigbee_router, and zigbee_ed_rx_off routines. I want to know how do I add the MAC address of the sender node to the packet when I broadcast, multicast, and unicast wireless data?(The default is the sender's network address) BR, Viki</description>
    <pubDate>Thu, 08 Apr 2021 03:44:17 GMT</pubDate>
    <dc:creator>Viki</dc:creator>
    <dc:date>2021-04-08T03:44:17Z</dc:date>
    <item>
      <title>JN5189 send data</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-send-data/m-p/1258507#M10991</link>
      <description>Hi All, The chip I use is JN5189, and the SDK version I use is SDK2.6.2_JN5189. I developed based on the zigbee_coordinator,zigbee_router, and zigbee_ed_rx_off routines. I want to know how do I add the MAC address of the sender node to the packet when I broadcast, multicast, and unicast wireless data?(The default is the sender's network address) BR, Viki</description>
      <pubDate>Thu, 08 Apr 2021 03:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-send-data/m-p/1258507#M10991</guid>
      <dc:creator>Viki</dc:creator>
      <dc:date>2021-04-08T03:44:17Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 send data</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-send-data/m-p/1259240#M11001</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Please refer the 'JN-UG-3130-Zigbee3-Stack.pdf', chapter 5.5. It is in the directory 'JN5189DK6.zip\docs\wireless\Zigbee'&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 09 Apr 2021 01:57:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-send-data/m-p/1259240#M11001</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-04-09T01:57:52Z</dc:date>
    </item>
  </channel>
</rss>