<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FIFO on CLRC632 in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/FIFO-on-CLRC632/m-p/1248770#M10926</link>
    <description>&lt;P&gt;If I wait for Idle command between write operations, CLRC632 works better. Now FIFO only contains one byte.&lt;/P&gt;</description>
    <pubDate>Fri, 19 Mar 2021 09:04:48 GMT</pubDate>
    <dc:creator>jbertrand</dc:creator>
    <dc:date>2021-03-19T09:04:48Z</dc:date>
    <item>
      <title>FIFO on CLRC632</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FIFO-on-CLRC632/m-p/1248405#M10923</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to write some functions to read ISO14443a tag with a CLRC632. I have written several functions to read and write registers, to read and write fifo and I'm pretty sure these functions are bug free as I can send a frame to FIFO, compute CRC code and read this CRC code from FIFO (with of course expected value).&lt;/P&gt;&lt;P&gt;Now, I'm triying to transceive a short frame (REQA). My function doesn't work and I have added some traces.&lt;/P&gt;&lt;LI-CODE lang="c"&gt;uint8_t
iso14443a_transceive_short_frame(uint8_t commande, iso14443a_atqa_t *atqa)
{
    uint8_t             longueur;

char t[40];
sprintf(t, "%d ", clrc632_read_register(CmdFIFOLength));

    // 7 bits, sans parité
    clrc632_write_register(CmdCommand, C_Idle);
sprintf(t, "%s%d ", t, clrc632_read_register(CmdFIFOLength));
    clrc632_write_register(RfChannelRedundancy, 0x00);
sprintf(t, "%s%d ", t, clrc632_read_register(CmdFIFOLength));
    clrc632_write_register(CtrlBitFraming, 7);
sprintf(t, "%s%d ", t, clrc632_read_register(CmdFIFOLength));

    memset(atqa, 0, sizeof(*atqa));

sprintf(t, "%s%d ", t, clrc632_read_register(CmdFIFOLength));
    clrc632_write(CmdFIFOData, (uint8_t *) &amp;amp;commande, sizeof(commande));
sprintf(t, "%s%d ", t, clrc632_read_register(CmdFIFOLength));
    clrc632_write_register(CmdCommand, C_Transceive);

sprintf(t, "%s%d\n\r", t, clrc632_read_register(CmdFIFOLength));
vfd_send_byte(0x0C);
vfd_print(t);
    longueur = 0;
    hz_set_t0(hz_timeout_nfc);

    do
    {
        if ((longueur = clrc632_read_register(CmdFIFOLength)) == 2)
        {
            break;
        }
    } while(hz_get_ts(hz_timeout_nfc) &amp;lt;= 5);

    if (longueur == 2)
    {
        (*atqa).data[0] = CmdFIFOData;
        (*atqa).data[1] = 0x00;

        clrc632_read((*atqa).data, longueur);

        sprintf(t, "%02X %02X", (*atqa).data[0], (*atqa).data[1]);
        vfd_print(t);
    }
    else
    {
        sprintf(t, "EL=%u", longueur);
        vfd_print(t);
    }

    clrc632_write_register(CmdCommand, C_Idle);
    return(ISO14443A_EXIT_SUCCESS);
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;Of course, CRLC632 is initialized before this function. I have read datasheet and, for me, this code only pushs one byte in FIFO (0x26).&lt;/P&gt;&lt;P&gt;vfd_printf() prints informations on a VFD sreen and I can see :&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;0 0 1 1 1 2 1
EL=0&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;I don't understand why clrc632_write_register(RfChannelRedundancy, 0x00) writes a byte in FIFO. I have verified that RfChannelRedundancy value is 0x22. Please note that, after clrc632_write(CmdFIFOData, (uint8_t *) &amp;amp;commande, sizeof(commande)), another byte is written in FIFO (0x26).&lt;/P&gt;&lt;P&gt;I suppose I have misunderstood something. Explanation will be welcome.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;JB&lt;/P&gt;</description>
      <pubDate>Thu, 18 Mar 2021 20:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FIFO-on-CLRC632/m-p/1248405#M10923</guid>
      <dc:creator>jbertrand</dc:creator>
      <dc:date>2021-03-18T20:58:53Z</dc:date>
    </item>
    <item>
      <title>Re: FIFO on CLRC632</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FIFO-on-CLRC632/m-p/1248770#M10926</link>
      <description>&lt;P&gt;If I wait for Idle command between write operations, CLRC632 works better. Now FIFO only contains one byte.&lt;/P&gt;</description>
      <pubDate>Fri, 19 Mar 2021 09:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FIFO-on-CLRC632/m-p/1248770#M10926</guid>
      <dc:creator>jbertrand</dc:creator>
      <dc:date>2021-03-19T09:04:48Z</dc:date>
    </item>
  </channel>
</rss>