<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CLRC663 + NxpNfcRdLib FCC Testing in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/CLRC663-NxpNfcRdLib-FCC-Testing/m-p/1246696#M10906</link>
    <description>&lt;P&gt;Are there instructions or examples for placing the CLRC663 in CW transmit mode for FCC testing? I found phhalHw_Rc663_Cmd_PRBS() but also discovered other pre-configurations are necessary. For example, the waterlevel register must be explicitly configured and the field must be manually switched on.&lt;/P&gt;&lt;P&gt;Is anything else necessary or recommended?&lt;/P&gt;</description>
    <pubDate>Tue, 16 Mar 2021 22:55:39 GMT</pubDate>
    <dc:creator>mraines</dc:creator>
    <dc:date>2021-03-16T22:55:39Z</dc:date>
    <item>
      <title>CLRC663 + NxpNfcRdLib FCC Testing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/CLRC663-NxpNfcRdLib-FCC-Testing/m-p/1246696#M10906</link>
      <description>&lt;P&gt;Are there instructions or examples for placing the CLRC663 in CW transmit mode for FCC testing? I found phhalHw_Rc663_Cmd_PRBS() but also discovered other pre-configurations are necessary. For example, the waterlevel register must be explicitly configured and the field must be manually switched on.&lt;/P&gt;&lt;P&gt;Is anything else necessary or recommended?&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 22:55:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/CLRC663-NxpNfcRdLib-FCC-Testing/m-p/1246696#M10906</guid>
      <dc:creator>mraines</dc:creator>
      <dc:date>2021-03-16T22:55:39Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 + NxpNfcRdLib FCC Testing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/CLRC663-NxpNfcRdLib-FCC-Testing/m-p/1253289#M10957</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182526"&gt;@mraines&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is no ready example for CLRC663 regarding FCC testing, but there is an example based on PN7150 for this topic, you may use it as a reference. Please kindly refer to&amp;nbsp;&lt;A href="https://github.com/NXP/nfc-linux_NfcFactoryTestApp" target="_blank"&gt;https://github.com/NXP/nfc-linux_NfcFactoryTestApp&lt;/A&gt;&amp;nbsp;for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Mar 2021 03:36:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/CLRC663-NxpNfcRdLib-FCC-Testing/m-p/1253289#M10957</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-03-29T03:36:46Z</dc:date>
    </item>
  </channel>
</rss>