<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: sniffer for thread</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/sniffer-for-thread/m-p/1244328#M10874</link>
    <description>&lt;P&gt;To add also that recent versions&amp;nbsp;of the KPAA Protocol Analyzer Adapter windows tool (latest &lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=Kinetis_Protocol_Analyzer_Adapter_2.0.4.1&amp;amp;appType=file1&amp;amp;location=null&amp;amp;DOWNLOAD_ID=null" target="_self"&gt;version 2.0.4.1&lt;/A&gt;) introduced support for simple tunneling of 802.15.4 packets from the&amp;nbsp;&lt;SPAN&gt;OM15080-K32W or OM15080-JN5189 running sniffer firmware into a Wireshark instance in order to do Thread packet capture.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 11 Mar 2021 18:15:22 GMT</pubDate>
    <dc:creator>Alin</dc:creator>
    <dc:date>2021-03-11T18:15:22Z</dc:date>
    <item>
      <title>sniffer for thread</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/sniffer-for-thread/m-p/1243322#M10867</link>
      <description>Hi NXP, I have some OM15080-K32W dongle. I am using them in Thread wireless network, typically as a Border Router, can it also be used as packet sniffer for thread? with Wireshark or ubiqua ? I noticed that the USB-KW41Z can be used as a packet sniffer with Wireshark: &lt;A href="https://www.nxp.com.cn/document/guide/get-started-with-the-usb-kw41z:NGS-USB-KW41Z" target="_blank"&gt;https://www.nxp.com.cn/document/guide/get-started-with-the-usb-kw41z:NGS-USB-KW41Z&lt;/A&gt; I have some 5169 dongle,too. but it seems like it can get zigbee packet only . Can you share a way to get the thread packet? Thanks.</description>
      <pubDate>Wed, 10 Mar 2021 14:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/sniffer-for-thread/m-p/1243322#M10867</guid>
      <dc:creator>Edward5</dc:creator>
      <dc:date>2021-03-10T14:14:57Z</dc:date>
    </item>
    <item>
      <title>Re: sniffer for thread</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/sniffer-for-thread/m-p/1243600#M10870</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184340"&gt;@Edward5&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing great.&lt;/P&gt;
&lt;P&gt;Thread is based&amp;nbsp;on IEEE® 802.15.4 MAC and PHY operating in the 2.4 GHz open radio frequency band. So in this case, it is part of the encryption and the application layer, in this case, Ubiqua provides the support to capture the Thread Traffic.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mario_castaneda_0-1615404887821.png" style="width: 473px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/139302iD04B0E3DDAEC0ECB/image-dimensions/473x236?v=v2" width="473" height="236" role="button" title="mario_castaneda_0-1615404887821.png" alt="mario_castaneda_0-1615404887821.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;mario_castaneda_0-1615404887821.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Mario&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 19:35:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/sniffer-for-thread/m-p/1243600#M10870</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2021-03-10T19:35:21Z</dc:date>
    </item>
    <item>
      <title>Re: sniffer for thread</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/sniffer-for-thread/m-p/1244328#M10874</link>
      <description>&lt;P&gt;To add also that recent versions&amp;nbsp;of the KPAA Protocol Analyzer Adapter windows tool (latest &lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=Kinetis_Protocol_Analyzer_Adapter_2.0.4.1&amp;amp;appType=file1&amp;amp;location=null&amp;amp;DOWNLOAD_ID=null" target="_self"&gt;version 2.0.4.1&lt;/A&gt;) introduced support for simple tunneling of 802.15.4 packets from the&amp;nbsp;&lt;SPAN&gt;OM15080-K32W or OM15080-JN5189 running sniffer firmware into a Wireshark instance in order to do Thread packet capture.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Mar 2021 18:15:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/sniffer-for-thread/m-p/1244328#M10874</guid>
      <dc:creator>Alin</dc:creator>
      <dc:date>2021-03-11T18:15:22Z</dc:date>
    </item>
  </channel>
</rss>