<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックBluetooth connection issue in imxul</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Bluetooth-connection-issue-in-imxul/m-p/1238581#M10821</link>
    <description>&lt;P&gt;Hi We are working on imx6ul. There is an issue with bluetooth connection , as we are able to pair, scan but not able to connect with bluetooth devices&lt;/P&gt;&lt;P&gt;below are the logs&lt;/P&gt;&lt;P&gt;root@imx6ulevk:~# bluetoothctl&lt;BR /&gt;Agent registered&lt;BR /&gt;[bluetooth]# scan on&lt;BR /&gt;Discovery started&lt;BR /&gt;[CHG] Controller D4:53:83:05:49:D5 Discovering: yes&lt;BR /&gt;[NEW] Device 70:BB:E9:4C:C5:79 Redmib&lt;BR /&gt;[NEW] Device 70:1C:E7:96:52:11 90100--IOT--GGN&lt;BR /&gt;[bluetooth]# scan off&lt;BR /&gt;Discovery stopped&lt;BR /&gt;[CHG] Controller D4:53:83:05:49:D5 Discovering: no&lt;BR /&gt;[CHG] Device 70:1C:E7:96:52:11 TxPower is nil&lt;BR /&gt;[CHG] Device 70:1C:E7:96:52:11 RSSI is nil&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 RSSI is nil&lt;BR /&gt;[bluetooth]# pair 70:BB:E9:4C:C5:79&lt;BR /&gt;Attempting to pair with 70:BB:E9:4C:C5:79&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 Connected: yes&lt;BR /&gt;Request PIN code&lt;BR /&gt;[agent] Enter PIN code: 1234&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 Modalias: bluetooth:v000Fp1200d1436&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001105-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000110a-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000110c-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000110e-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001112-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001115-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001116-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000111f-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000112d-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000112f-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001132-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001200-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001800-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001801-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 98b97136-36a2-11ea-8467-484d7e99a198&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 ServicesResolved: yes&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 Paired: yes&lt;BR /&gt;Pairing successful&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 ServicesResolved: no&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 Connected: no&lt;BR /&gt;[bluetooth]# connect 70:BB:E9:4C:C5:79&lt;BR /&gt;Attempting to connect to 70:BB:E9:4C:C5:79&lt;BR /&gt;Failed to connect: org.bluez.Error.Failed&lt;BR /&gt;[bluetooth]#&lt;/P&gt;&lt;P&gt;Kindly help&lt;/P&gt;</description>
    <pubDate>Tue, 02 Mar 2021 09:14:25 GMT</pubDate>
    <dc:creator>bulkesh</dc:creator>
    <dc:date>2021-03-02T09:14:25Z</dc:date>
    <item>
      <title>Bluetooth connection issue in imxul</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Bluetooth-connection-issue-in-imxul/m-p/1238581#M10821</link>
      <description>&lt;P&gt;Hi We are working on imx6ul. There is an issue with bluetooth connection , as we are able to pair, scan but not able to connect with bluetooth devices&lt;/P&gt;&lt;P&gt;below are the logs&lt;/P&gt;&lt;P&gt;root@imx6ulevk:~# bluetoothctl&lt;BR /&gt;Agent registered&lt;BR /&gt;[bluetooth]# scan on&lt;BR /&gt;Discovery started&lt;BR /&gt;[CHG] Controller D4:53:83:05:49:D5 Discovering: yes&lt;BR /&gt;[NEW] Device 70:BB:E9:4C:C5:79 Redmib&lt;BR /&gt;[NEW] Device 70:1C:E7:96:52:11 90100--IOT--GGN&lt;BR /&gt;[bluetooth]# scan off&lt;BR /&gt;Discovery stopped&lt;BR /&gt;[CHG] Controller D4:53:83:05:49:D5 Discovering: no&lt;BR /&gt;[CHG] Device 70:1C:E7:96:52:11 TxPower is nil&lt;BR /&gt;[CHG] Device 70:1C:E7:96:52:11 RSSI is nil&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 RSSI is nil&lt;BR /&gt;[bluetooth]# pair 70:BB:E9:4C:C5:79&lt;BR /&gt;Attempting to pair with 70:BB:E9:4C:C5:79&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 Connected: yes&lt;BR /&gt;Request PIN code&lt;BR /&gt;[agent] Enter PIN code: 1234&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 Modalias: bluetooth:v000Fp1200d1436&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001105-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000110a-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000110c-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000110e-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001112-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001115-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001116-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000111f-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000112d-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000112f-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001132-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001200-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001800-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001801-0000-1000-8000-00805f9b34fb&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 98b97136-36a2-11ea-8467-484d7e99a198&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 ServicesResolved: yes&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 Paired: yes&lt;BR /&gt;Pairing successful&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 ServicesResolved: no&lt;BR /&gt;[CHG] Device 70:BB:E9:4C:C5:79 Connected: no&lt;BR /&gt;[bluetooth]# connect 70:BB:E9:4C:C5:79&lt;BR /&gt;Attempting to connect to 70:BB:E9:4C:C5:79&lt;BR /&gt;Failed to connect: org.bluez.Error.Failed&lt;BR /&gt;[bluetooth]#&lt;/P&gt;&lt;P&gt;Kindly help&lt;/P&gt;</description>
      <pubDate>Tue, 02 Mar 2021 09:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Bluetooth-connection-issue-in-imxul/m-p/1238581#M10821</guid>
      <dc:creator>bulkesh</dc:creator>
      <dc:date>2021-03-02T09:14:25Z</dc:date>
    </item>
    <item>
      <title>Re: Bluetooth connection issue in imxul</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Bluetooth-connection-issue-in-imxul/m-p/1240345#M10836</link>
      <description>&lt;P&gt;hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please help me with the Bluetooth part you are using ?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Estephania&lt;/P&gt;</description>
      <pubDate>Thu, 04 Mar 2021 15:48:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Bluetooth-connection-issue-in-imxul/m-p/1240345#M10836</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2021-03-04T15:48:55Z</dc:date>
    </item>
  </channel>
</rss>