<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: JN5189 wakeup in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-wakeup/m-p/1236101#M10811</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181842"&gt;@Viki&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing great.&lt;/P&gt;
&lt;P&gt;I recommend looking at the JN-AN-1246 that could help you with the implementation of the button and also the routines that the code implements.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Mario&lt;/P&gt;</description>
    <pubDate>Wed, 24 Feb 2021 20:58:25 GMT</pubDate>
    <dc:creator>mario_castaneda</dc:creator>
    <dc:date>2021-02-24T20:58:25Z</dc:date>
    <item>
      <title>JN5189 wakeup</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-wakeup/m-p/1235332#M10802</link>
      <description>&lt;P&gt;Hi All，&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;The chip I use is JN5189, the SDK version I use is SDK2.6.2_JN5189DK6, and the routine I use is Zigbee_ed_rx_off.&lt;BR /&gt;The default setting of this routine can realize the timing wake-up of the device. In addition, I hope to realize that when the module is sleeping, press the wake-up button to immediately wake up the device, and when the wake-up button is released, the module will continue to sleep in accordance with the sleep cycle.&lt;BR /&gt;How to realize this function?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;BR，&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;Viki&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Feb 2021 02:46:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-wakeup/m-p/1235332#M10802</guid>
      <dc:creator>Viki</dc:creator>
      <dc:date>2021-02-24T02:46:24Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 wakeup</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-wakeup/m-p/1236101#M10811</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181842"&gt;@Viki&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing great.&lt;/P&gt;
&lt;P&gt;I recommend looking at the JN-AN-1246 that could help you with the implementation of the button and also the routines that the code implements.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Mario&lt;/P&gt;</description>
      <pubDate>Wed, 24 Feb 2021 20:58:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-wakeup/m-p/1236101#M10811</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2021-02-24T20:58:25Z</dc:date>
    </item>
  </channel>
</rss>