<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic vAHI_SwReset() API, which will trigger a Leave in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/vAHI-SwReset-API-which-will-trigger-a-Leave/m-p/1234600#M10787</link>
    <description>&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;We are currently maintaining a&amp;nbsp; Zigbee controller out of JN5169.&lt;BR /&gt;We are using the JN-SW-4170 SDK.&lt;BR /&gt;We have of course a good understanding of JN-AN-1216&lt;BR /&gt;Application Note: JN-AN-1216 ZigBee 3.0 IoT Control Bridge,&lt;BR /&gt;as well as the JN-UG-3113 User Guide section B.5&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;We detect a strange behaviour after calling vAHI_SwReset(), indeed after such call any devices which is in the Child Table receive from the Controller a Leave message&lt;/P&gt;&lt;P&gt;Is there an expected behaviour ?&lt;/P&gt;&lt;P&gt;Is there a configuration to disable such behaviour and prevent the Leave message to be issued ?&lt;/P&gt;</description>
    <pubDate>Mon, 22 Feb 2021 22:02:11 GMT</pubDate>
    <dc:creator>zigbee1</dc:creator>
    <dc:date>2021-02-22T22:02:11Z</dc:date>
    <item>
      <title>vAHI_SwReset() API, which will trigger a Leave</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/vAHI-SwReset-API-which-will-trigger-a-Leave/m-p/1234600#M10787</link>
      <description>&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;We are currently maintaining a&amp;nbsp; Zigbee controller out of JN5169.&lt;BR /&gt;We are using the JN-SW-4170 SDK.&lt;BR /&gt;We have of course a good understanding of JN-AN-1216&lt;BR /&gt;Application Note: JN-AN-1216 ZigBee 3.0 IoT Control Bridge,&lt;BR /&gt;as well as the JN-UG-3113 User Guide section B.5&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;We detect a strange behaviour after calling vAHI_SwReset(), indeed after such call any devices which is in the Child Table receive from the Controller a Leave message&lt;/P&gt;&lt;P&gt;Is there an expected behaviour ?&lt;/P&gt;&lt;P&gt;Is there a configuration to disable such behaviour and prevent the Leave message to be issued ?&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 22:02:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/vAHI-SwReset-API-which-will-trigger-a-Leave/m-p/1234600#M10787</guid>
      <dc:creator>zigbee1</dc:creator>
      <dc:date>2021-02-22T22:02:11Z</dc:date>
    </item>
    <item>
      <title>Re: vAHI_SwReset() API, which will trigger a Leave</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/vAHI-SwReset-API-which-will-trigger-a-Leave/m-p/1235172#M10800</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;vAHI_SwReset.&amp;nbsp;&lt;/SPAN&gt;This reset has the same effect as pulling the&amp;nbsp;external RESETN line low and is likely to result in the loss of&amp;nbsp;the contents of on-chip RAM&lt;/P&gt;
&lt;P&gt;Do you have a sniffer log about this behavior?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Mario&lt;/P&gt;</description>
      <pubDate>Tue, 23 Feb 2021 19:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/vAHI-SwReset-API-which-will-trigger-a-Leave/m-p/1235172#M10800</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2021-02-23T19:05:56Z</dc:date>
    </item>
  </channel>
</rss>