<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic JN5189 GPIO in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-GPIO/m-p/1233961#M10777</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;The chip I use is JN5189, the SDK version I use is SDK2.6.2_JN5189DK6, and the routine I use is Zigbee_ed_rx_on.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;I wanted to use the PIO21 pin as a general GPIO output (function 1 of PIO21 is a function of GPIO) and I found that after calling GPIO_PinInit() and IOCON_PinMuxSet() to set it to function 1, I still couldn't control its output low level properly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;&lt;SPAN&gt;It is worth mentioning that the above method can control the PIO7 output high/low level normally.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;I want to know how to control the normal output of PIO21 high/low level?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;BR,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;Viki&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sun, 21 Feb 2021 08:05:00 GMT</pubDate>
    <dc:creator>Viki</dc:creator>
    <dc:date>2021-02-21T08:05:00Z</dc:date>
    <item>
      <title>JN5189 GPIO</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-GPIO/m-p/1233961#M10777</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;The chip I use is JN5189, the SDK version I use is SDK2.6.2_JN5189DK6, and the routine I use is Zigbee_ed_rx_on.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;I wanted to use the PIO21 pin as a general GPIO output (function 1 of PIO21 is a function of GPIO) and I found that after calling GPIO_PinInit() and IOCON_PinMuxSet() to set it to function 1, I still couldn't control its output low level properly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;&lt;SPAN&gt;It is worth mentioning that the above method can control the PIO7 output high/low level normally.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;I want to know how to control the normal output of PIO21 high/low level?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;BR,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;Viki&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 21 Feb 2021 08:05:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-GPIO/m-p/1233961#M10777</guid>
      <dc:creator>Viki</dc:creator>
      <dc:date>2021-02-21T08:05:00Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 GPIO</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-GPIO/m-p/1234018#M10778</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I use led demo to test the pin. I only add two code to control the pin. It works.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137649i214B7B24A26BF294/image-size/medium?v=v2&amp;amp;px=400" role="button" title="1.PNG" alt="1.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 01:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-GPIO/m-p/1234018#M10778</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-02-22T01:57:06Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 GPIO</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-GPIO/m-p/1234193#M10782</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/71004"&gt;@nxf56274&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;I observe that you are controlling the high output level of the PIO21 pin.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;&lt;SPAN class="transSent"&gt;As my question says, I can control the PIO21 pin to output high levels, but I can't control it to output low levels.&lt;/SPAN&gt;&lt;SPAN class="transSent"&gt;May I ask if the PIO21 pin can normally output low level in your test?&lt;/SPAN&gt;&lt;SPAN class="transSent"&gt;Are the chips and SDK versions you use the same as mine?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;BR,&lt;/P&gt;&lt;P class="_tgt transPara grammarSection"&gt;Viki&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 07:46:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-GPIO/m-p/1234193#M10782</guid>
      <dc:creator>Viki</dc:creator>
      <dc:date>2021-02-22T07:46:04Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 GPIO</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-GPIO/m-p/1234210#M10783</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Both are OK. The sdk is the latest.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 08:22:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-GPIO/m-p/1234210#M10783</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-02-22T08:22:26Z</dc:date>
    </item>
  </channel>
</rss>