<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Simplified API example for DESFire missing from the NFC reader library. in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Simplified-API-example-for-DESFire-missing-from-the-NFC-reader/m-p/1229884#M10746</link>
    <description>&lt;DIV class="page"&gt;&lt;DIV class="layoutArea"&gt;&lt;DIV class="column"&gt;&lt;P&gt;&lt;SPAN&gt;There should be a Simplified API ISO example for MIFARE DESFire as is stated in AN11022 at 6.12 and in AN11802 at 5.1.9.&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;In the reader library I have downloaded there is a function prototype, but no actual function definition.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In the main code body there is a print out that it is not supported contrary to what the ANs state.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE&gt;case E_PH_NFCLIB_MIFARE_DESFIRE:&lt;BR /&gt;   DEBUG_PRINTF (" \nMifare Desfire detected... \n");&lt;BR /&gt;   DEBUG_PRINTF (" \nMifare Desfire not supported in simplified api... \n");&lt;BR /&gt;   break;&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I run this example for the DESFire card?&lt;BR /&gt;&lt;BR /&gt;Also after following the instructions to build example files in AN11902 on raspberry pi, scripts only generates half of the examples listed as available. Examples 2, 7, 10 and 11 are missing. How do I get the rest of them?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Thu, 11 Feb 2021 13:30:49 GMT</pubDate>
    <dc:creator>Seagull_Island</dc:creator>
    <dc:date>2021-02-11T13:30:49Z</dc:date>
    <item>
      <title>Simplified API example for DESFire missing from the NFC reader library.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Simplified-API-example-for-DESFire-missing-from-the-NFC-reader/m-p/1229884#M10746</link>
      <description>&lt;DIV class="page"&gt;&lt;DIV class="layoutArea"&gt;&lt;DIV class="column"&gt;&lt;P&gt;&lt;SPAN&gt;There should be a Simplified API ISO example for MIFARE DESFire as is stated in AN11022 at 6.12 and in AN11802 at 5.1.9.&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;In the reader library I have downloaded there is a function prototype, but no actual function definition.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In the main code body there is a print out that it is not supported contrary to what the ANs state.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE&gt;case E_PH_NFCLIB_MIFARE_DESFIRE:&lt;BR /&gt;   DEBUG_PRINTF (" \nMifare Desfire detected... \n");&lt;BR /&gt;   DEBUG_PRINTF (" \nMifare Desfire not supported in simplified api... \n");&lt;BR /&gt;   break;&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I run this example for the DESFire card?&lt;BR /&gt;&lt;BR /&gt;Also after following the instructions to build example files in AN11902 on raspberry pi, scripts only generates half of the examples listed as available. Examples 2, 7, 10 and 11 are missing. How do I get the rest of them?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 11 Feb 2021 13:30:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Simplified-API-example-for-DESFire-missing-from-the-NFC-reader/m-p/1229884#M10746</guid>
      <dc:creator>Seagull_Island</dc:creator>
      <dc:date>2021-02-11T13:30:49Z</dc:date>
    </item>
    <item>
      <title>Re: Simplified API example for DESFire missing from the NFC reader library.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Simplified-API-example-for-DESFire-missing-from-the-NFC-reader/m-p/1235131#M10799</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As you might know,&amp;nbsp; there are some of the documents and libraries which are under NDA (Non-Disclosure Agreement) and placed in &lt;A href="https://www.docstore.nxp.com/" target="_self"&gt;Docstore&lt;/A&gt;, the information of the DesFire technology is located under NDA in the system. &lt;/P&gt;
&lt;P&gt;Please , help me check &lt;A href="https://community.nxp.com/t5/NFC/MIFARE-DESFire-in-the-PN7462AU-FW-and-SW-examples-Full-version-v/m-p/754175" target="_self"&gt;this&lt;/A&gt; post as a reference.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Estephania&lt;/P&gt;</description>
      <pubDate>Tue, 23 Feb 2021 17:51:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Simplified-API-example-for-DESFire-missing-from-the-NFC-reader/m-p/1235131#M10799</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2021-02-23T17:51:34Z</dc:date>
    </item>
  </channel>
</rss>