<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NT3H2111/2211, I2C to NFC address translation for SRAM_MIRROR_BLOCK in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/NT3H2111-2211-I2C-to-NFC-address-translation-for-SRAM-MIRROR/m-p/1217461#M10600</link>
    <description>&lt;P&gt;Yes,&amp;nbsp; Thank you for the clarification.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
    <pubDate>Wed, 20 Jan 2021 00:43:57 GMT</pubDate>
    <dc:creator>cabletie</dc:creator>
    <dc:date>2021-01-20T00:43:57Z</dc:date>
    <item>
      <title>NT3H2111/2211, I2C to NFC address translation for SRAM_MIRROR_BLOCK</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NT3H2111-2211-I2C-to-NFC-address-translation-for-SRAM-MIRROR/m-p/1212469#M10575</link>
      <description>&lt;P&gt;prevous thread:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Wireless-Connectivity/NT3H2111-2211-SRAM-MIRROR-BLOCK-I2C-to-NFC-address-translation/m-p/1201908" target="_blank"&gt;https://community.nxp.com/t5/Wireless-Connectivity/NT3H2111-2211-SRAM-MIRROR-BLOCK-I2C-to-NFC-address-translation/m-p/1201908&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I still need clarification on HOW the SRAM_MIRROR_BLOCK address value TRANSLATES&lt;/P&gt;&lt;P&gt;into the NFC side address. The datasheet only indicates the NFC-side address&lt;/P&gt;&lt;P&gt;as 0x04 for the I2C side address value of 0x01. (the page(s) size/block size not-with-standing)&lt;/P&gt;&lt;P&gt;So, when the SRAM_MIRROR_BLOCK address value is 0x01 the NFC side address is 0x04;&lt;/P&gt;&lt;P&gt;but how about when the SRAM_MIRROR_BLOCK address value is set to 0x02?&lt;BR /&gt;--&amp;gt; what does the NFC-side address value become? and...&lt;/P&gt;&lt;P&gt;for address value set to 0x03? --&amp;gt; what does the NFC-side address value become? etc.&lt;/P&gt;&lt;P&gt;I guess basically I am asking how far (address value increments) does the&lt;/P&gt;&lt;P&gt;NFC-side beginning SRAM byte move (address-wise) for a SRAM_MIRROR_BLOCK value change?&lt;/P&gt;&lt;P&gt;I hope this helps to understand my question. Perhaps the attached picture will help?&lt;/P&gt;&lt;P&gt;(( I suppose it goes without saying a hole in the memory OR the end of the&lt;/P&gt;&lt;P&gt;memory bound needs to be respected when moving the SRAM location toward&lt;/P&gt;&lt;P&gt;the end of the SECTION. ))&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jan 2021 16:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NT3H2111-2211-I2C-to-NFC-address-translation-for-SRAM-MIRROR/m-p/1212469#M10575</guid>
      <dc:creator>cabletie</dc:creator>
      <dc:date>2021-01-15T16:18:16Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111/2211, I2C to NFC address translation for SRAM_MIRROR_BLOCK</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NT3H2111-2211-I2C-to-NFC-address-translation-for-SRAM-MIRROR/m-p/1216491#M10592</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You may refer to the table 13 as the datasheet. Example in the table.&amp;nbsp; the value of SRAM_MIRROR_BLOCK is 34h.&amp;nbsp; The value of NFC page is D0H for NTAG I2C pluse 1K. Please refer to the attachment how to transfer it .&lt;/P&gt;
&lt;P&gt;Hope it help you. Have a nice day.&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 03:35:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NT3H2111-2211-I2C-to-NFC-address-translation-for-SRAM-MIRROR/m-p/1216491#M10592</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-01-19T03:35:11Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111/2211, I2C to NFC address translation for SRAM_MIRROR_BLOCK</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NT3H2111-2211-I2C-to-NFC-address-translation-for-SRAM-MIRROR/m-p/1217461#M10600</link>
      <description>&lt;P&gt;Yes,&amp;nbsp; Thank you for the clarification.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 00:43:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NT3H2111-2211-I2C-to-NFC-address-translation-for-SRAM-MIRROR/m-p/1217461#M10600</guid>
      <dc:creator>cabletie</dc:creator>
      <dc:date>2021-01-20T00:43:57Z</dc:date>
    </item>
  </channel>
</rss>