<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic JN5168-M05 in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/JN5168-M05/m-p/497987#M1055</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just started using a high powered JN5168-M05 for a project. Whilst it is running and sending out debug information the radio does not seem to be working at all. It does not link to a coordinator, and when it does an energy scan (as a coordinator) all the energies come back as 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using it in basic IEEE15.4 mode. &lt;/P&gt;&lt;P&gt;The same code works find on a M00 module.&lt;/P&gt;&lt;P&gt;I have called &lt;/P&gt;&lt;P&gt;vAppApiSetHighPowerMode( APP_API_MODULE_HPM05, TRUE ) before using radio.&lt;/P&gt;&lt;P&gt;I am using it with an external 2dB dipole antenna.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have downloaded the NXP JN-AP-1172 JN516x Customer Module Evaluation Tool. I've compiled it in BeYond Studio with the latest SDK.&lt;/P&gt;&lt;P&gt;The results are similar : When I run it on a M00 and do the receive test or RF power measurement test I can see activity on the channels.&lt;/P&gt;&lt;P&gt;When I run the same binary (and enable high power mode from the terminal) on a M05 the channels are completely silent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Its like the radio is not switched on in the M05.&lt;/P&gt;&lt;P&gt;I have tried two M05.&lt;/P&gt;&lt;P&gt;I have used the M00 module extensively without issue.&lt;/P&gt;&lt;P&gt;Antenna is not shorted or anything like that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone got an M05 working? Any ideas what I could be doing wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for any help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Jan 2016 16:49:32 GMT</pubDate>
    <dc:creator>hazeman</dc:creator>
    <dc:date>2016-01-18T16:49:32Z</dc:date>
    <item>
      <title>JN5168-M05</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5168-M05/m-p/497987#M1055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just started using a high powered JN5168-M05 for a project. Whilst it is running and sending out debug information the radio does not seem to be working at all. It does not link to a coordinator, and when it does an energy scan (as a coordinator) all the energies come back as 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using it in basic IEEE15.4 mode. &lt;/P&gt;&lt;P&gt;The same code works find on a M00 module.&lt;/P&gt;&lt;P&gt;I have called &lt;/P&gt;&lt;P&gt;vAppApiSetHighPowerMode( APP_API_MODULE_HPM05, TRUE ) before using radio.&lt;/P&gt;&lt;P&gt;I am using it with an external 2dB dipole antenna.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have downloaded the NXP JN-AP-1172 JN516x Customer Module Evaluation Tool. I've compiled it in BeYond Studio with the latest SDK.&lt;/P&gt;&lt;P&gt;The results are similar : When I run it on a M00 and do the receive test or RF power measurement test I can see activity on the channels.&lt;/P&gt;&lt;P&gt;When I run the same binary (and enable high power mode from the terminal) on a M05 the channels are completely silent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Its like the radio is not switched on in the M05.&lt;/P&gt;&lt;P&gt;I have tried two M05.&lt;/P&gt;&lt;P&gt;I have used the M00 module extensively without issue.&lt;/P&gt;&lt;P&gt;Antenna is not shorted or anything like that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone got an M05 working? Any ideas what I could be doing wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for any help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 16:49:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5168-M05/m-p/497987#M1055</guid>
      <dc:creator>hazeman</dc:creator>
      <dc:date>2016-01-18T16:49:32Z</dc:date>
    </item>
    <item>
      <title>Re: JN5168-M05</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5168-M05/m-p/497988#M1056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ignore this - I was driving 5V into DIO1. It was configured as an input so but 5V is over voltage.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jan 2016 14:45:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5168-M05/m-p/497988#M1056</guid>
      <dc:creator>hazeman</dc:creator>
      <dc:date>2016-01-19T14:45:10Z</dc:date>
    </item>
    <item>
      <title>Re: JN5168-M05</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5168-M05/m-p/497989#M1057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am also working on JN5168-001-M06. Can u plz tell me ho or where to get the beyond studio IDE and SDks.&lt;/P&gt;&lt;P&gt;I am really stuck. Plz help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jul 2016 13:53:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5168-M05/m-p/497989#M1057</guid>
      <dc:creator>vivekpjohn</dc:creator>
      <dc:date>2016-07-04T13:53:45Z</dc:date>
    </item>
    <item>
      <title>Re: JN5168-M05</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5168-M05/m-p/497990#M1058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Calling the makers and experts interested in using Zigbee via NXP JN5168 modules, please join the facebook group so we can help each other:)&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fgoo.gl%2FDeYbC6" rel="nofollow" target="_blank"&gt;https://goo.gl/DeYbC6&lt;/A&gt;&lt;BR /&gt;Cheers&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Sep 2017 16:28:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5168-M05/m-p/497990#M1058</guid>
      <dc:creator>adamjacob</dc:creator>
      <dc:date>2017-09-11T16:28:12Z</dc:date>
    </item>
  </channel>
</rss>