<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: qn9080sip</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/qn9080sip/m-p/1183281#M10372</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;It is possible that a phone could connect to a multiple QN9080. Just you have to be sure of the role that the phone and the QN9080 are taking and if the Phone supports multiple connections as well.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Mario&lt;/P&gt;</description>
    <pubDate>Fri, 13 Nov 2020 18:27:52 GMT</pubDate>
    <dc:creator>mario_castaneda</dc:creator>
    <dc:date>2020-11-13T18:27:52Z</dc:date>
    <item>
      <title>qn9080sip</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/qn9080sip/m-p/1182792#M10370</link>
      <description>&lt;P&gt;&lt;FONT&gt;Can a mobile phone connect with multiple qn9080 Bluetooth devices? And why?&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Nov 2020 04:43:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/qn9080sip/m-p/1182792#M10370</guid>
      <dc:creator>1758793535</dc:creator>
      <dc:date>2020-11-13T04:43:09Z</dc:date>
    </item>
    <item>
      <title>Re: qn9080sip</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/qn9080sip/m-p/1183281#M10372</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;It is possible that a phone could connect to a multiple QN9080. Just you have to be sure of the role that the phone and the QN9080 are taking and if the Phone supports multiple connections as well.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Mario&lt;/P&gt;</description>
      <pubDate>Fri, 13 Nov 2020 18:27:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/qn9080sip/m-p/1183281#M10372</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2020-11-13T18:27:52Z</dc:date>
    </item>
  </channel>
</rss>