<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic kw41z wireless uart hasn't characteristic value. in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/kw41z-wireless-uart-hasn-t-characteristic-value/m-p/1180778#M10362</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i merge a ble stack code from project wirelessuartdemo-like to other project with the same mcu board (kw41z).&lt;/P&gt;&lt;P&gt;The first project work correctly. I can send and receive data with iotToolbox.&lt;/P&gt;&lt;P&gt;The new project instead has a problem: The device can receive a message but can't respond to smartphone.&lt;/P&gt;&lt;P&gt;To send data i use&amp;nbsp;GattClient_WriteCharacteristicValue() that want&amp;nbsp;gattCharacteristic_t type between varoius parameters.&lt;/P&gt;&lt;P&gt;Before it i assign&amp;nbsp;characteristic.value.handle = mPeerInformation.clientInfo.hUartStream; but the problem is that mPeerInformation.clientInfo.hUartStream is zero. In the functioning code, this is not zero so if i overwrite characteristic.value.handle with the correct value it work fine.&lt;/P&gt;&lt;P&gt;i looked for mPeerInformation assignment and i found only one function that is&amp;nbsp; BleApp_StoreServiceHandles() but the break point don't stop to it in any project. How is it possible?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 10 Nov 2020 12:45:07 GMT</pubDate>
    <dc:creator>mangramarco</dc:creator>
    <dc:date>2020-11-10T12:45:07Z</dc:date>
    <item>
      <title>kw41z wireless uart hasn't characteristic value.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/kw41z-wireless-uart-hasn-t-characteristic-value/m-p/1180778#M10362</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i merge a ble stack code from project wirelessuartdemo-like to other project with the same mcu board (kw41z).&lt;/P&gt;&lt;P&gt;The first project work correctly. I can send and receive data with iotToolbox.&lt;/P&gt;&lt;P&gt;The new project instead has a problem: The device can receive a message but can't respond to smartphone.&lt;/P&gt;&lt;P&gt;To send data i use&amp;nbsp;GattClient_WriteCharacteristicValue() that want&amp;nbsp;gattCharacteristic_t type between varoius parameters.&lt;/P&gt;&lt;P&gt;Before it i assign&amp;nbsp;characteristic.value.handle = mPeerInformation.clientInfo.hUartStream; but the problem is that mPeerInformation.clientInfo.hUartStream is zero. In the functioning code, this is not zero so if i overwrite characteristic.value.handle with the correct value it work fine.&lt;/P&gt;&lt;P&gt;i looked for mPeerInformation assignment and i found only one function that is&amp;nbsp; BleApp_StoreServiceHandles() but the break point don't stop to it in any project. How is it possible?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Nov 2020 12:45:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/kw41z-wireless-uart-hasn-t-characteristic-value/m-p/1180778#M10362</guid>
      <dc:creator>mangramarco</dc:creator>
      <dc:date>2020-11-10T12:45:07Z</dc:date>
    </item>
    <item>
      <title>Re: kw41z wireless uart hasn't characteristic value.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/kw41z-wireless-uart-hasn-t-characteristic-value/m-p/1181152#M10366</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This means your mcu doesn't find the phone's service. Check why the mcu doesn't find the service.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 11 Nov 2020 02:34:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/kw41z-wireless-uart-hasn-t-characteristic-value/m-p/1181152#M10366</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2020-11-11T02:34:46Z</dc:date>
    </item>
  </channel>
</rss>