<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FRDM-KW41Z Development board - Onboard RX/TX voltage level in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Development-board-Onboard-RX-TX-voltage-level/m-p/1176049#M10339</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have just bought an&amp;nbsp;FRDM-KW41Z dev kit.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The dev board has an Arduino R3 compatible connector (for shields or individual cables).&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can not find if the serial RX/TX pins of this socket (HDR pin 1 (PTC6) and pin 2 (PTC7)) are TTL compatible or 3V3.&lt;/P&gt;&lt;P&gt;I see in the schematics that they are connected directly to the uP (MKW41Z512VHT4 MCU).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please, can anyone tell me which are the RX/TX voltage levels in such board?&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;David.&lt;/P&gt;</description>
    <pubDate>Fri, 30 Oct 2020 18:05:57 GMT</pubDate>
    <dc:creator>dvdsosa</dc:creator>
    <dc:date>2020-10-30T18:05:57Z</dc:date>
    <item>
      <title>FRDM-KW41Z Development board - Onboard RX/TX voltage level</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Development-board-Onboard-RX-TX-voltage-level/m-p/1176049#M10339</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have just bought an&amp;nbsp;FRDM-KW41Z dev kit.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The dev board has an Arduino R3 compatible connector (for shields or individual cables).&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can not find if the serial RX/TX pins of this socket (HDR pin 1 (PTC6) and pin 2 (PTC7)) are TTL compatible or 3V3.&lt;/P&gt;&lt;P&gt;I see in the schematics that they are connected directly to the uP (MKW41Z512VHT4 MCU).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please, can anyone tell me which are the RX/TX voltage levels in such board?&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;David.&lt;/P&gt;</description>
      <pubDate>Fri, 30 Oct 2020 18:05:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Development-board-Onboard-RX-TX-voltage-level/m-p/1176049#M10339</guid>
      <dc:creator>dvdsosa</dc:creator>
      <dc:date>2020-10-30T18:05:57Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KW41Z Development board - Onboard RX/TX voltage level</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Development-board-Onboard-RX-TX-voltage-level/m-p/1176425#M10344</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;david_sosa,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; PTC6, PTC7 which is the UART0-TX and UART_RX pin, it is the 3.3V TTL pin.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;So, you also can find a TTL-USB tool to connect that pin, please note, the TTL-USB tool also need to provide the 3.3V to the UART TLL pins.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Wish it helps you!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you still have questions about it, please kindly let me know!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Note:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;-----------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Nov 2020 06:25:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Development-board-Onboard-RX-TX-voltage-level/m-p/1176425#M10344</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2020-11-02T06:25:39Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KW41Z Development board - Onboard RX/TX voltage level</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Development-board-Onboard-RX-TX-voltage-level/m-p/1176514#M10345</link>
      <description>&lt;P&gt;Hello Kerry,&lt;/P&gt;&lt;P&gt;I'm sorry, but with your answer, I still have the doubt.&lt;/P&gt;&lt;P&gt;Given that TTL is 5V (it is not the same as 3.3V), then, at which voltage works the UART from the FRDM-KW41Z? 5V or 3.3V?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David.&lt;/P&gt;</description>
      <pubDate>Mon, 02 Nov 2020 08:52:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Development-board-Onboard-RX-TX-voltage-level/m-p/1176514#M10345</guid>
      <dc:creator>dvdsosa</dc:creator>
      <dc:date>2020-11-02T08:52:00Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KW41Z Development board - Onboard RX/TX voltage level</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Development-board-Onboard-RX-TX-voltage-level/m-p/1176551#M10347</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;david_sosa,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; KW41 is 3.3V.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; As I know, some TTL-USB tool can select 3.3V, this is an example:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 684px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128822i9A3982467408DE53/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;image.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Mon, 02 Nov 2020 09:39:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Development-board-Onboard-RX-TX-voltage-level/m-p/1176551#M10347</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2020-11-02T09:39:30Z</dc:date>
    </item>
  </channel>
</rss>