<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピック[88W8987]: Labtool CMD32</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/88W8987-Labtool-CMD32/m-p/1172983#M10317</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i have a couple of questions regarding the 88W8987 WLAN SoC in an RX test scenario in combination with the Labtool command CMD32.&lt;/P&gt;&lt;P&gt;CMD32 returns the packetCount, multicastCount and the errorCount.&lt;/P&gt;&lt;P&gt;I would like to measure the "receiver minimum input sensitivity" (unit: dBm) for an arbitrary IEEE standard, modulation, coding rate and frequency band, which are send to the 88W8987 WLAN SoC.&lt;/P&gt;&lt;P&gt;In the document ApplicationNote_LabtoolUserGuide_88W8987_-_Vx, January 2019.pdf various RX test scenarios are listed with the CMD32 as last step.&lt;/P&gt;&lt;P&gt;Is there a way to calculate the "receiver minimum input sensitivity" (unit dBm) from the CMD32 returned packet statistics?&lt;/P&gt;&lt;P&gt;Also:&lt;/P&gt;&lt;P&gt;CMD198 and CMD199 return the RSSI values.&lt;/P&gt;&lt;P&gt;Could you provide a RX test scenario similar to the ones in the Labtool user guide with these commands?&lt;/P&gt;&lt;P&gt;Because executing these instead of CMD32 just returns 0.&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;</description>
    <pubDate>Mon, 26 Oct 2020 08:52:51 GMT</pubDate>
    <dc:creator>DanielVector111</dc:creator>
    <dc:date>2020-10-26T08:52:51Z</dc:date>
    <item>
      <title>[88W8987]: Labtool CMD32</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/88W8987-Labtool-CMD32/m-p/1172983#M10317</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i have a couple of questions regarding the 88W8987 WLAN SoC in an RX test scenario in combination with the Labtool command CMD32.&lt;/P&gt;&lt;P&gt;CMD32 returns the packetCount, multicastCount and the errorCount.&lt;/P&gt;&lt;P&gt;I would like to measure the "receiver minimum input sensitivity" (unit: dBm) for an arbitrary IEEE standard, modulation, coding rate and frequency band, which are send to the 88W8987 WLAN SoC.&lt;/P&gt;&lt;P&gt;In the document ApplicationNote_LabtoolUserGuide_88W8987_-_Vx, January 2019.pdf various RX test scenarios are listed with the CMD32 as last step.&lt;/P&gt;&lt;P&gt;Is there a way to calculate the "receiver minimum input sensitivity" (unit dBm) from the CMD32 returned packet statistics?&lt;/P&gt;&lt;P&gt;Also:&lt;/P&gt;&lt;P&gt;CMD198 and CMD199 return the RSSI values.&lt;/P&gt;&lt;P&gt;Could you provide a RX test scenario similar to the ones in the Labtool user guide with these commands?&lt;/P&gt;&lt;P&gt;Because executing these instead of CMD32 just returns 0.&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 08:52:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/88W8987-Labtool-CMD32/m-p/1172983#M10317</guid>
      <dc:creator>DanielVector111</dc:creator>
      <dc:date>2020-10-26T08:52:51Z</dc:date>
    </item>
    <item>
      <title>Re: [88W8987]: Labtool CMD32</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/88W8987-Labtool-CMD32/m-p/1174686#M10334</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;
&lt;P&gt;I hope you are doing great.&lt;/P&gt;
&lt;P&gt;Did you solve your issue? Did you get the&amp;nbsp;&lt;SPAN&gt;receiver minimum input sensitivity?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Mario&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Oct 2020 18:24:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/88W8987-Labtool-CMD32/m-p/1174686#M10334</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2020-10-28T18:24:29Z</dc:date>
    </item>
  </channel>
</rss>