<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Writing multiple tags (NTAG) with PC in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Writing-multiple-tags-NTAG-with-PC/m-p/1170294#M10289</link>
    <description>&lt;P&gt;Knowing that there is a solution for a mobile phone device to write multiple tags in a row, I would like to ask if there is a ready solution for PC (using a reader/writer) to write multiple tags and record/log their data (UID and status) for future use.&lt;/P&gt;&lt;P&gt;Is there a ready solution using the TagXplorer or any ready script for the action?&lt;/P&gt;&lt;P&gt;The purpose is to have a conveyor attached to the reader/writer to be able to set the same info and settings to all the NTAG213 tags by passing them by the writer.&lt;/P&gt;</description>
    <pubDate>Tue, 20 Oct 2020 10:41:17 GMT</pubDate>
    <dc:creator>MikhailUz</dc:creator>
    <dc:date>2020-10-20T10:41:17Z</dc:date>
    <item>
      <title>Writing multiple tags (NTAG) with PC</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Writing-multiple-tags-NTAG-with-PC/m-p/1170294#M10289</link>
      <description>&lt;P&gt;Knowing that there is a solution for a mobile phone device to write multiple tags in a row, I would like to ask if there is a ready solution for PC (using a reader/writer) to write multiple tags and record/log their data (UID and status) for future use.&lt;/P&gt;&lt;P&gt;Is there a ready solution using the TagXplorer or any ready script for the action?&lt;/P&gt;&lt;P&gt;The purpose is to have a conveyor attached to the reader/writer to be able to set the same info and settings to all the NTAG213 tags by passing them by the writer.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 10:41:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Writing-multiple-tags-NTAG-with-PC/m-p/1170294#M10289</guid>
      <dc:creator>MikhailUz</dc:creator>
      <dc:date>2020-10-20T10:41:17Z</dc:date>
    </item>
    <item>
      <title>Re: Writing multiple tags (NTAG) with PC</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Writing-multiple-tags-NTAG-with-PC/m-p/1170512#M10292</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We have several readers that can achieve the purpose, it will depend on the tag protocol you are using the reader to use,. You can check our available readers in &lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers:NFC-READER" target="_self"&gt;this&lt;/A&gt; page.&lt;/P&gt;
&lt;P&gt;In this case, we do not have a ready solution as requested, there is the need for every customer to implement their application , still, you can check as well in the &lt;A href="https://www.nxp.com/products/rfid-nfc/rfid-ecosystem:RFID_ECOSYSTEMS" target="_self"&gt;RFID Ecosystem&lt;/A&gt; for a solution provider for your needs.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Estephania&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 18:52:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Writing-multiple-tags-NTAG-with-PC/m-p/1170512#M10292</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2020-10-20T18:52:32Z</dc:date>
    </item>
  </channel>
</rss>