<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic AFT05MP075 in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/AFT05MP075/m-p/1153716#M10150</link>
    <description>&lt;P&gt;I use ADS simulated AFT05MP075 results is not like the datasheet Figure 3 Drain current verse Drain-Source Voltage，I want to know if it is a datasheet error or simulation error.&lt;/P&gt;</description>
    <pubDate>Wed, 16 Sep 2020 00:57:00 GMT</pubDate>
    <dc:creator>yunwang666</dc:creator>
    <dc:date>2020-09-16T00:57:00Z</dc:date>
    <item>
      <title>AFT05MP075</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/AFT05MP075/m-p/1153716#M10150</link>
      <description>&lt;P&gt;I use ADS simulated AFT05MP075 results is not like the datasheet Figure 3 Drain current verse Drain-Source Voltage，I want to know if it is a datasheet error or simulation error.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Sep 2020 00:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/AFT05MP075/m-p/1153716#M10150</guid>
      <dc:creator>yunwang666</dc:creator>
      <dc:date>2020-09-16T00:57:00Z</dc:date>
    </item>
    <item>
      <title>Re: AFT05MP075</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/AFT05MP075/m-p/1156383#M10168</link>
      <description>&lt;P&gt;AFT05MP075 ADS model has been optimized to match measured RF performance.&lt;/P&gt;
&lt;P&gt;DC parameter was not specially tuned. In fact, most of the difference between datasheet Figure 3 and simulation is determined by different gate threshold voltages of the model and of the datasheet instance. This value is about 0.5V more in the model vs datasheet sample.&lt;/P&gt;
&lt;P&gt;Note 1. Gate threshold voltage can differ from sample to sample due to production spread. Datasheet specifies VGS(th)=[1.7,2.5]V. Figure 3 was measured on the device with VGS(th)~2V whereas the threshold in the model is closer to 2.5V.&lt;/P&gt;
&lt;P&gt;Note 2. The accuracy of DC model is not critical, since the gate bias voltage of each device has to be tuned individually.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Pavel&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2020 16:44:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/AFT05MP075/m-p/1156383#M10168</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2020-09-21T16:44:46Z</dc:date>
    </item>
  </channel>
</rss>