<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックConfiguring the DAC: DACREF_1 pin</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Configuring-the-DAC-DACREF-1-pin/m-p/251138#M956</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm configuring the DAC on the Vybrid, and noticed a reference (Reference Manual, rev4) to DACREF as the voltage input. However, I haven't been able to find this pin on the Vybrid schematic (F-series, RevG), or on Vybrid_Pinout_1.1_-_F_Series.xlsx.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Jul 2013 18:52:26 GMT</pubDate>
    <dc:creator>n00b1024</dc:creator>
    <dc:date>2013-07-02T18:52:26Z</dc:date>
    <item>
      <title>Configuring the DAC: DACREF_1 pin</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Configuring-the-DAC-DACREF-1-pin/m-p/251138#M956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm configuring the DAC on the Vybrid, and noticed a reference (Reference Manual, rev4) to DACREF as the voltage input. However, I haven't been able to find this pin on the Vybrid schematic (F-series, RevG), or on Vybrid_Pinout_1.1_-_F_Series.xlsx.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2013 18:52:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Configuring-the-DAC-DACREF-1-pin/m-p/251138#M956</guid>
      <dc:creator>n00b1024</dc:creator>
      <dc:date>2013-07-02T18:52:26Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring the DAC: DACREF_1 pin</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Configuring-the-DAC-DACREF-1-pin/m-p/251139#M957</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Those are internal connections to the DAC module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following will be in the next revision of the RM:&lt;/P&gt;&lt;P&gt;For this device, external voltage supplied to VREFH_ADC pin is the only reference voltage for DAC reference.&lt;/P&gt;&lt;P&gt;User will need to set up DACx_STATCTRL [DACRFS]=1 to select the valid VREFH_ADC reference.&lt;/P&gt;&lt;P&gt;When DACx_STATCTRL [DACRFS]=0, the DAC reference is connected to an internal ground node and is not a valid voltage reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Anthony&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2013 18:59:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Configuring-the-DAC-DACREF-1-pin/m-p/251139#M957</guid>
      <dc:creator>anthony_huereca</dc:creator>
      <dc:date>2013-07-02T18:59:59Z</dc:date>
    </item>
  </channel>
</rss>