<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TWR-VF65GS10 OpenSDA serial error in uboot in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/TWR-VF65GS10-OpenSDA-serial-error-in-uboot/m-p/248908#M923</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you ran the OOBE demo, this in Linux/MQX on both cores, each with a dedicated serial port, one using the TWR-SER, the other using the Virtual Serial Port, both running at 115200, I can't say I've noticed errors when using that, you can also use the jumpers on the rev G boards to swap the serial ports over so put A5 to TWR-SER or VSP to test bigger traffic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems unlikely, but have you tried re-programming the app, or have you been able to test a second board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ross&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Aug 2013 10:25:30 GMT</pubDate>
    <dc:creator>RossMcLuckie</dc:creator>
    <dc:date>2013-08-20T10:25:30Z</dc:date>
    <item>
      <title>TWR-VF65GS10 OpenSDA serial error in uboot</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/TWR-VF65GS10-OpenSDA-serial-error-in-uboot/m-p/248906#M921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone come across uboot serial errors over OpenSDA (at 115200bps) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The error does not exist at lower baud rates, in Linux, or if the TWR-SER interface is used for Cortex-A5 console output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Aug 2013 14:39:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/TWR-VF65GS10-OpenSDA-serial-error-in-uboot/m-p/248906#M921</guid>
      <dc:creator>michaelleung</dc:creator>
      <dc:date>2013-08-11T14:39:56Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-VF65GS10 OpenSDA serial error in uboot</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/TWR-VF65GS10-OpenSDA-serial-error-in-uboot/m-p/248907#M922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Correction : the serial errors happen in Linux over OpenSDA too. So it looks like s CDC problem in OpenSDA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Aug 2013 21:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/TWR-VF65GS10-OpenSDA-serial-error-in-uboot/m-p/248907#M922</guid>
      <dc:creator>michaelleung</dc:creator>
      <dc:date>2013-08-11T21:15:30Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-VF65GS10 OpenSDA serial error in uboot</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/TWR-VF65GS10-OpenSDA-serial-error-in-uboot/m-p/248908#M923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you ran the OOBE demo, this in Linux/MQX on both cores, each with a dedicated serial port, one using the TWR-SER, the other using the Virtual Serial Port, both running at 115200, I can't say I've noticed errors when using that, you can also use the jumpers on the rev G boards to swap the serial ports over so put A5 to TWR-SER or VSP to test bigger traffic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems unlikely, but have you tried re-programming the app, or have you been able to test a second board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ross&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Aug 2013 10:25:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/TWR-VF65GS10-OpenSDA-serial-error-in-uboot/m-p/248908#M923</guid>
      <dc:creator>RossMcLuckie</dc:creator>
      <dc:date>2013-08-20T10:25:30Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-VF65GS10 OpenSDA serial error in uboot</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/TWR-VF65GS10-OpenSDA-serial-error-in-uboot/m-p/248909#M924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ross,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the default board configuration using OpenSDA for SCI UART, you will see errors in u-boot (eg the response to help command), or the console output when you boot linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I swap jumpers so that SCI1 comes out to primary elevator (UART1) and to TWR-SER, there is no error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem seems to be in OpenSDA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you look into it please ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 31 Aug 2013 17:28:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/TWR-VF65GS10-OpenSDA-serial-error-in-uboot/m-p/248909#M924</guid>
      <dc:creator>michaelleung</dc:creator>
      <dc:date>2013-08-31T17:28:30Z</dc:date>
    </item>
  </channel>
</rss>