<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックVybrid PWM</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-PWM/m-p/246803#M859</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all, I'm just starting to go through the Vybrid documentation, specifically the VF6.&amp;nbsp; I know it is early, and that the documentation isn't very complete so far.&amp;nbsp; My interest this minute is a PWM generator.&amp;nbsp; I need a PWM to adjust the brightness of several indicator LEDs in my design.&amp;nbsp;&amp;nbsp; The datasheet doesn't mention PWM at all, but it appears that the VF6 uses a timer peripheral similar to those used on Kinetis parts that do claim PWM capability.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using very efficient LEDs such that when all are turned on full brightness the draw is only 300uA.&amp;nbsp; My battery powered device needs long life, and sleeps for long periods of time.&amp;nbsp; So, I need any PWM that I use as little power as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming the VF6 does have PWM capability, here are my questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. How much duty cycle control do I have?&lt;/P&gt;&lt;P&gt;2. Can the low power timer be used to generate PWM?&lt;/P&gt;&lt;P&gt;3. Which of the low power modes allows the PWM to generate (I want my LEDs lit when the design is sleeping).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 30 Jun 2013 18:56:36 GMT</pubDate>
    <dc:creator>johnfielden</dc:creator>
    <dc:date>2013-06-30T18:56:36Z</dc:date>
    <item>
      <title>Vybrid PWM</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-PWM/m-p/246803#M859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all, I'm just starting to go through the Vybrid documentation, specifically the VF6.&amp;nbsp; I know it is early, and that the documentation isn't very complete so far.&amp;nbsp; My interest this minute is a PWM generator.&amp;nbsp; I need a PWM to adjust the brightness of several indicator LEDs in my design.&amp;nbsp;&amp;nbsp; The datasheet doesn't mention PWM at all, but it appears that the VF6 uses a timer peripheral similar to those used on Kinetis parts that do claim PWM capability.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using very efficient LEDs such that when all are turned on full brightness the draw is only 300uA.&amp;nbsp; My battery powered device needs long life, and sleeps for long periods of time.&amp;nbsp; So, I need any PWM that I use as little power as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming the VF6 does have PWM capability, here are my questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. How much duty cycle control do I have?&lt;/P&gt;&lt;P&gt;2. Can the low power timer be used to generate PWM?&lt;/P&gt;&lt;P&gt;3. Which of the low power modes allows the PWM to generate (I want my LEDs lit when the design is sleeping).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Jun 2013 18:56:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-PWM/m-p/246803#M859</guid>
      <dc:creator>johnfielden</dc:creator>
      <dc:date>2013-06-30T18:56:36Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid PWM</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-PWM/m-p/246804#M860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello John,&lt;/P&gt;&lt;P&gt;As a hardware person, I cannot comment on the PWM specifics, but based on my experience, any processor with a timer does it one way or the other.&lt;/P&gt;&lt;P&gt;At the same time, I can comment on the power consumption optimization for your battery-powered application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First you have to formulate your power consumption requirements, based on the battery capacity.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then you have to lower the processor's power consumption by:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;using the lowest possible reference clock frequency,&lt;/LI&gt;&lt;LI&gt;turning all the unnecessary processor's blocks OFF (see power domains for them),&lt;/LI&gt;&lt;LI&gt;select the Low-Power stop mode suitable for your application,&lt;/LI&gt;&lt;LI&gt;optimize the power management scheme (linear, based on external NPN transistor),&lt;/LI&gt;&lt;LI&gt;etc.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Feel free to come with follow-up questions.&lt;/P&gt;&lt;P&gt;Sincerely, Naoum Gitnik.&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jul 2013 21:01:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-PWM/m-p/246804#M860</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2013-07-12T21:01:05Z</dc:date>
    </item>
  </channel>
</rss>