<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can I boot using QuadSPI from QSPI1? in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Can-I-boot-using-QuadSPI-from-QSPI1/m-p/241979#M644</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Richard,&lt;/P&gt;&lt;P&gt;The details of your application are a bit unclear, but, please, take a look at another discussion in which you might find an answer - &lt;A _jive_internal="true" href="https://community.nxp.com/thread/309836"&gt;https://community.freescale.com/thread/309836.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Regards, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Aug 2013 23:10:38 GMT</pubDate>
    <dc:creator>naoumgitnik</dc:creator>
    <dc:date>2013-08-06T23:10:38Z</dc:date>
    <item>
      <title>Can I boot using QuadSPI from QSPI1?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Can-I-boot-using-QuadSPI-from-QSPI1/m-p/241978#M643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I know it is possible to boot using QSPI0, with one or two flash chips. But is it possible to boot using QSPI1?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Aug 2013 09:27:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Can-I-boot-using-QuadSPI-from-QSPI1/m-p/241978#M643</guid>
      <dc:creator>richarddonkin</dc:creator>
      <dc:date>2013-08-06T09:27:14Z</dc:date>
    </item>
    <item>
      <title>Re: Can I boot using QuadSPI from QSPI1?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Can-I-boot-using-QuadSPI-from-QSPI1/m-p/241979#M644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Richard,&lt;/P&gt;&lt;P&gt;The details of your application are a bit unclear, but, please, take a look at another discussion in which you might find an answer - &lt;A _jive_internal="true" href="https://community.nxp.com/thread/309836"&gt;https://community.freescale.com/thread/309836.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Regards, Naoum Gitnik.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Aug 2013 23:10:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Can-I-boot-using-QuadSPI-from-QSPI1/m-p/241979#M644</guid>
      <dc:creator>naoumgitnik</dc:creator>
      <dc:date>2013-08-06T23:10:38Z</dc:date>
    </item>
    <item>
      <title>Re: Can I boot using QuadSPI from QSPI1?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Can-I-boot-using-QuadSPI-from-QSPI1/m-p/241980#M645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you can. Note however that you cannot use parallel mode with QuadSPI1 as there are not the pins for it on the chip. If you want to use parallel (8-bit) mode, you must use QuadSPI0. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2013 20:39:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Can-I-boot-using-QuadSPI-from-QSPI1/m-p/241980#M645</guid>
      <dc:creator>anthony_huereca</dc:creator>
      <dc:date>2013-08-07T20:39:11Z</dc:date>
    </item>
    <item>
      <title>Re: Can I boot using QuadSPI from QSPI1?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Can-I-boot-using-QuadSPI-from-QSPI1/m-p/241981#M646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the clear response!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2013 04:58:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Can-I-boot-using-QuadSPI-from-QSPI1/m-p/241981#M646</guid>
      <dc:creator>richarddonkin</dc:creator>
      <dc:date>2013-08-08T04:58:25Z</dc:date>
    </item>
  </channel>
</rss>