<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic This an automatic process.  We are marking this post as s... in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Maximum-NAND-flash/m-p/1138642#M6148</link>
    <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
    <pubDate>Thu, 03 Sep 2020 18:57:01 GMT</pubDate>
    <dc:creator>CommunityBot</dc:creator>
    <dc:date>2020-09-03T18:57:01Z</dc:date>
    <item>
      <title>Maximum NAND flash.</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Maximum-NAND-flash/m-p/499176#M5388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello I am investigating the reference manual for Vybrid processor R-series. I am tiring to find the is there are limitations for the maximum size of the NAND flash connected to the Vybrid. Do you have any recommendations about using 512MB NAND?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Dec 2015 08:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Maximum-NAND-flash/m-p/499176#M5388</guid>
      <dc:creator>gelkov</dc:creator>
      <dc:date>2015-12-22T08:34:01Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum NAND flash.</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Maximum-NAND-flash/m-p/499177#M5389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Maxim,&lt;/P&gt;&lt;P&gt;NAND flashes use 5 cycle addressing:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33593iA01275CE5052834D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In NFC you can select address by:&lt;/P&gt;&lt;P&gt;column NFC_CAR - 2 bytes&lt;/P&gt;&lt;P&gt;row NFC_RAR - 3 bytes + 2 CS.&lt;/P&gt;&lt;P&gt;So theoretically it is really big memory.&lt;/P&gt;&lt;P&gt;No official recommendation for 512MB. On TWR-VF65 we use MT29F2G16ABAEAWP:E 256MB (2Gb).&lt;/P&gt;&lt;P&gt;/Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 08:48:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Maximum-NAND-flash/m-p/499177#M5389</guid>
      <dc:creator>jiri-b36968</dc:creator>
      <dc:date>2016-01-12T08:48:40Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Maximum-NAND-flash/m-p/1138642#M6148</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 18:57:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Maximum-NAND-flash/m-p/1138642#M6148</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T18:57:01Z</dc:date>
    </item>
  </channel>
</rss>