<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックThis an automatic process.  We are marking this post as s...</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/USB-DMA-request-fails/m-p/1137936#M6123</link>
    <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
    <pubDate>Thu, 03 Sep 2020 17:41:56 GMT</pubDate>
    <dc:creator>CommunityBot</dc:creator>
    <dc:date>2020-09-03T17:41:56Z</dc:date>
    <item>
      <title>USB DMA request fails</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-DMA-request-fails/m-p/453289#M5042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;currently we have problems with usb dma. If I read data with the cpu from the receive buffer of the usb dma, while the usb dma stremas data into it, the received data are corrupted.&lt;/P&gt;&lt;P&gt;My questions are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the priority of the usb dma transfer on the ahb bus?&lt;/P&gt;&lt;P&gt;I started to read the doc of the NIC301 and I saw that there are QoS values which refelcts the priority of the bus masters. How can I check these&lt;/P&gt;&lt;P&gt;Qos values and where can I modify these?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-&amp;gt; Info on 07/29/2015: I found out that the data cache is enable for the RX Buffer. But in the MQX driver code the data ache lines of the&lt;/P&gt;&lt;P&gt;rx buffer are flushed before the dma request is started. It seems to me that the flushing of the data cache line is not sufficient in this case?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Dirk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nachricht geändert durch Dirk Schmitt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 05:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-DMA-request-fails/m-p/453289#M5042</guid>
      <dc:creator>dirkschmitt</dc:creator>
      <dc:date>2015-07-28T05:29:41Z</dc:date>
    </item>
    <item>
      <title>Re: USB DMA request fails</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-DMA-request-fails/m-p/453290#M5043</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I have seen the priorities of the NIC remain the same and do not change.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can get access to the &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;NIC&lt;/STRONG&gt;&lt;/SPAN&gt; registers via:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define NIC301_BASE_PTR ((NIC301_MemMapPtr)0x40008000u)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which MQX version are you using? I know that latest release solved a few issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2015 19:10:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-DMA-request-fails/m-p/453290#M5043</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-08-10T19:10:58Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/USB-DMA-request-fails/m-p/1137936#M6123</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 17:41:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/USB-DMA-request-fails/m-p/1137936#M6123</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T17:41:56Z</dc:date>
    </item>
  </channel>
</rss>