<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックUsing QSPI1 interface on VF3XXR devices</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Using-QSPI1-interface-on-VF3XXR-devices/m-p/678704#M5833</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are designing a board for the VF3XXR R Series Vybrid, probably the SVF311R3K1CKU2.&lt;/P&gt;&lt;P&gt;Our hardware engineer is planning to use QSPI1 based on the functionality listed in the Pinouts table 12.1 in the R Series Datasheet "VYBRIDRSERIESEC.pdf" - VYBRIDRSERIESEC Rev 7, 11/2014.&lt;/P&gt;&lt;P&gt;For example, on page 92 it lists QFP pin 47 as having ALT7 functionality of "QSPI1_A_SCK" and ditto for pins 49 to 55.&lt;/P&gt;&lt;P&gt;However, looking at the Device Configuration table on p.143 of the Vybrid Reference Manual, it lists the VF3XXR device as having only 1 Quad SPI.&lt;/P&gt;&lt;P&gt;Does this mean we can only use QSPI0 on the VF3XXR devices, even though the ALT7 functionality is listed in the pinout table for the R- Series ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Jul 2017 13:49:42 GMT</pubDate>
    <dc:creator>martinbell</dc:creator>
    <dc:date>2017-07-21T13:49:42Z</dc:date>
    <item>
      <title>Using QSPI1 interface on VF3XXR devices</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Using-QSPI1-interface-on-VF3XXR-devices/m-p/678704#M5833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are designing a board for the VF3XXR R Series Vybrid, probably the SVF311R3K1CKU2.&lt;/P&gt;&lt;P&gt;Our hardware engineer is planning to use QSPI1 based on the functionality listed in the Pinouts table 12.1 in the R Series Datasheet "VYBRIDRSERIESEC.pdf" - VYBRIDRSERIESEC Rev 7, 11/2014.&lt;/P&gt;&lt;P&gt;For example, on page 92 it lists QFP pin 47 as having ALT7 functionality of "QSPI1_A_SCK" and ditto for pins 49 to 55.&lt;/P&gt;&lt;P&gt;However, looking at the Device Configuration table on p.143 of the Vybrid Reference Manual, it lists the VF3XXR device as having only 1 Quad SPI.&lt;/P&gt;&lt;P&gt;Does this mean we can only use QSPI0 on the VF3XXR devices, even though the ALT7 functionality is listed in the pinout table for the R- Series ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jul 2017 13:49:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Using-QSPI1-interface-on-VF3XXR-devices/m-p/678704#M5833</guid>
      <dc:creator>martinbell</dc:creator>
      <dc:date>2017-07-21T13:49:42Z</dc:date>
    </item>
  </channel>
</rss>