<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックVybrid multiple resets</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-multiple-resets/m-p/636154#M5756</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We use the KVF61NS152CMK50, but only the A5 core is used. We&amp;nbsp;observed some very strange behavior on the reset line after a short 3.3V dip &amp;nbsp;– see attached.&lt;/P&gt;&lt;P&gt;Blue trace is 3.3V, Yellow is /RESET&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The /RESET line is connected to the output of MCU supervisor MCP130. That circuit is attached as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What would be the reason for multiple resets after a brief loss of 3.3V power? Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Mar 2017 00:14:50 GMT</pubDate>
    <dc:creator>shouminliu</dc:creator>
    <dc:date>2017-03-09T00:14:50Z</dc:date>
    <item>
      <title>Vybrid multiple resets</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-multiple-resets/m-p/636154#M5756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We use the KVF61NS152CMK50, but only the A5 core is used. We&amp;nbsp;observed some very strange behavior on the reset line after a short 3.3V dip &amp;nbsp;– see attached.&lt;/P&gt;&lt;P&gt;Blue trace is 3.3V, Yellow is /RESET&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The /RESET line is connected to the output of MCU supervisor MCP130. That circuit is attached as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What would be the reason for multiple resets after a brief loss of 3.3V power? Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 00:14:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-multiple-resets/m-p/636154#M5756</guid>
      <dc:creator>shouminliu</dc:creator>
      <dc:date>2017-03-09T00:14:50Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid multiple resets</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-multiple-resets/m-p/636155#M5757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;It looks like that 3.3V is incorrect on your board. Your oscilloscope diagram shows that there is about 3.0V on your board. The MPC130 generates RESET since 3.3V is incorrect.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Check power supply on your board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 04:59:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-multiple-resets/m-p/636155#M5757</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-03-22T04:59:49Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid multiple resets</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-multiple-resets/m-p/636156#M5758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pavel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the comment. The 3.3V rail actually is in spec. Please refer to the attached screenshot. 3.3V did not go all the way down to ground (0V) before it came back up to 3.3V. Would this cause any problems?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have also observed that if 3.3V remains low for 1 second or so, Vybrid can be reset correctly and everything works fine. Is there a requirement that 3.3V has to be low for more than a certain period of time before POR can be done correctly? Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--SL&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2017 02:41:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-multiple-resets/m-p/636156#M5758</guid>
      <dc:creator>shouminliu</dc:creator>
      <dc:date>2017-03-24T02:41:57Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid multiple resets</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-multiple-resets/m-p/636157#M5759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Most of processors required that power voltage should go to 0V before &lt;SPAN style="color: black;"&gt;it came back up to 3.3V. This requirement is needed since processor use internal circuit for power up. This circuit is used for processor register initialization (resetting) at power up. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;It looks like that this Vybrid internal circuit goes to initial state if &lt;SPAN style="color: black;"&gt;3.3V remains low for 1 second or so.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2017 06:52:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-multiple-resets/m-p/636157#M5759</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-03-28T06:52:04Z</dc:date>
    </item>
  </channel>
</rss>