<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SPI - set inactive state of SOUT in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/SPI-set-inactive-state-of-SOUT/m-p/628396#M5740</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SPI on Vybrid can be configured through a dedicated set of registers.&lt;/P&gt;&lt;P&gt;Inactive state for PCS and SCK can be configured with PCSIS (in SPIx_MCR) and CPOL (in SPIx_CTARn).&lt;/P&gt;&lt;P&gt;I don't find a way to set the inactive state for SOUT, and with an oscilloscope I see that this is HIGH.&lt;/P&gt;&lt;P&gt;Is there a way to set it to LOW?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Mar 2017 08:14:11 GMT</pubDate>
    <dc:creator>vix</dc:creator>
    <dc:date>2017-03-07T08:14:11Z</dc:date>
    <item>
      <title>SPI - set inactive state of SOUT</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SPI-set-inactive-state-of-SOUT/m-p/628396#M5740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SPI on Vybrid can be configured through a dedicated set of registers.&lt;/P&gt;&lt;P&gt;Inactive state for PCS and SCK can be configured with PCSIS (in SPIx_MCR) and CPOL (in SPIx_CTARn).&lt;/P&gt;&lt;P&gt;I don't find a way to set the inactive state for SOUT, and with an oscilloscope I see that this is HIGH.&lt;/P&gt;&lt;P&gt;Is there a way to set it to LOW?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Mar 2017 08:14:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SPI-set-inactive-state-of-SOUT/m-p/628396#M5740</guid>
      <dc:creator>vix</dc:creator>
      <dc:date>2017-03-07T08:14:11Z</dc:date>
    </item>
    <item>
      <title>Re: SPI - set inactive state of SOUT</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SPI-set-inactive-state-of-SOUT/m-p/628397#M5741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no way of configuring the inactive state of the SOUT signal, it is always High.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Mar 2017 09:16:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SPI-set-inactive-state-of-SOUT/m-p/628397#M5741</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-03-27T09:16:17Z</dc:date>
    </item>
  </channel>
</rss>