<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: Vybrid DDR3 write leveling</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589690#M5676</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please pay attention on the Mark Middleton comments in &lt;BR /&gt;&lt;A href="https://community.nxp.com/thread/395323"&gt;Vybrid: About DDR leveling feature on DDRMC.&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"First, I want to make sure that we correctly define and understand the different timing parameters, because the IP we are using in Vybrid uses confusing terms:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Write Leveling (WRLVL_DL_0/1) refers to adjusting the timing between the Write DQS strobe signal and the SDCLK signals, so that the edges align.&lt;/LI&gt;&lt;LI&gt;DLL Write delay (DLL_WRITE_DL) refers to adjusting the DQS strobe in relation to the DQ signals so that the strobe edge is centered in the window of valid write data.&lt;/LI&gt;&lt;LI&gt;Read Leveling (RDLVL_DL_0/1) refers to adjusting the DQS strobe in relation to the DQ signals so that the strobe edge is&lt;BR /&gt;centered in the window of valid read data.&lt;/LI&gt;&lt;LI&gt;Read Gate Delay (RDLVL_GTDL_0/1) refers to the delay the PHY uses to un-gate the Read DQS strobe pad from the time that the PHY enables the pad to input the strobe signal.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;To help understand this last point, I am attaching an explanation I recently wrote that discusses Write and Read Latency timings and the settings used both for the DDR devices and for the PHY.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Second, the Vybrid DDR controller only supports training using a software mode controlled by the Memory Controller (Hardware Training is not supported by the PHY). NXP does not have any SW to perform Write Leveling because we do not expect customers to use memory in a Fly-By Topology. The total memory address space supported by Vybrid is easily accommodated by one or two DDR devices. Fly-By Topology is typically used for x64 and x128 bus widths.&lt;BR /&gt;Nevertheless, if the customer really wants to configure DDR3 in a Fly-By Topology, they can manually enter delay values into the WRLVL_DL_0/1 fields based on trace length differences from their layout. Mismatches up to 25% or tCK (clock period) are allowed, so the value in the filed doesn’t have to be very accurate."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the &lt;A href="https://community.nxp.com/thread/313817"&gt;DDR Stress test tuning&lt;/A&gt;&amp;nbsp; - I will send You recommendations via e-mail. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Aug 2016 06:09:43 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-08-01T06:09:43Z</dc:date>
    <item>
      <title>Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589685#M5671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are currently working on write leveling, gate training and read leveling on a Vybrid-based board with external DDR3 memory (Micron MT41K256M16HA-125 AIT:E). Unfortunately, we are unable to obtain any values for the rising edge using the procedures described in chapter 10.1.16 of the Vybrid Reference Manual (rev. 8).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First of all; it is not clear about the order of these procedures. Assuming that the manual list the procedures in the correct order, we have focused on getting the rising edge in write-leveling first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that, using table 10-25 (page 1593), we keep adjusting WRLVL_DL_X for data slices 0 and 1 until they reach zero. At this point, we terminate the leveling procedure, using 0x00 for the write leveling delay. The board boots with with this value, but it also boots without any leveling/training at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2016 06:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589685#M5671</guid>
      <dc:creator>tfe</dc:creator>
      <dc:date>2016-06-30T06:19:39Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589686#M5672</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/karinavalencia"&gt;karinavalencia&lt;/A&gt;​,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can we expect a response on this anytime soon?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jul 2016 07:32:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589686#M5672</guid>
      <dc:creator>tfe</dc:creator>
      <dc:date>2016-07-21T07:32:36Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589687#M5673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/SergioSolis"&gt;SergioSolis&lt;/A&gt;​ can you help here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jul 2016 14:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589687#M5673</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2016-07-21T14:30:43Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589688#M5674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I hope the following helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/395323"&gt;Vybrid: About DDR leveling feature on DDRMC.&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/328852"&gt;Is there a DDR3 stress test tool for the Vybrid processors?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/341868"&gt;Testing MT41J64M16JT-15E DDR Memory using PE DDrv Vybrid Validation Tool - How to Demo?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/313817"&gt;DDR Stress test tuning&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jul 2016 05:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589688#M5674</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-07-26T05:30:42Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589689#M5675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are already familiar wit the top two links, and they seem to focus on the DDR validation tool in Processor Expert. This tool is of no interest to us.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The two latter threads you are referencing are not accessible to us, stating "Unauthorized: Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you think these threads would be useful to our situation, could you the provide us access to these threads?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 09:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589689#M5675</guid>
      <dc:creator>tfe</dc:creator>
      <dc:date>2016-07-28T09:49:51Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589690#M5676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please pay attention on the Mark Middleton comments in &lt;BR /&gt;&lt;A href="https://community.nxp.com/thread/395323"&gt;Vybrid: About DDR leveling feature on DDRMC.&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"First, I want to make sure that we correctly define and understand the different timing parameters, because the IP we are using in Vybrid uses confusing terms:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Write Leveling (WRLVL_DL_0/1) refers to adjusting the timing between the Write DQS strobe signal and the SDCLK signals, so that the edges align.&lt;/LI&gt;&lt;LI&gt;DLL Write delay (DLL_WRITE_DL) refers to adjusting the DQS strobe in relation to the DQ signals so that the strobe edge is centered in the window of valid write data.&lt;/LI&gt;&lt;LI&gt;Read Leveling (RDLVL_DL_0/1) refers to adjusting the DQS strobe in relation to the DQ signals so that the strobe edge is&lt;BR /&gt;centered in the window of valid read data.&lt;/LI&gt;&lt;LI&gt;Read Gate Delay (RDLVL_GTDL_0/1) refers to the delay the PHY uses to un-gate the Read DQS strobe pad from the time that the PHY enables the pad to input the strobe signal.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;To help understand this last point, I am attaching an explanation I recently wrote that discusses Write and Read Latency timings and the settings used both for the DDR devices and for the PHY.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Second, the Vybrid DDR controller only supports training using a software mode controlled by the Memory Controller (Hardware Training is not supported by the PHY). NXP does not have any SW to perform Write Leveling because we do not expect customers to use memory in a Fly-By Topology. The total memory address space supported by Vybrid is easily accommodated by one or two DDR devices. Fly-By Topology is typically used for x64 and x128 bus widths.&lt;BR /&gt;Nevertheless, if the customer really wants to configure DDR3 in a Fly-By Topology, they can manually enter delay values into the WRLVL_DL_0/1 fields based on trace length differences from their layout. Mismatches up to 25% or tCK (clock period) are allowed, so the value in the filed doesn’t have to be very accurate."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the &lt;A href="https://community.nxp.com/thread/313817"&gt;DDR Stress test tuning&lt;/A&gt;&amp;nbsp; - I will send You recommendations via e-mail. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Aug 2016 06:09:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589690#M5676</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-08-01T06:09:43Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589691#M5677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our apologies if we did not make ourselves clear.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As mentioned: We are familiar with the comment and thread you are referencing. Hence we have updated our training-routines to reflect the corrections made in said thread, yet we still do not see any change in our results.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are also familiar with the document you sent me by e-mail. However this document is lacking the details we need to progress.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Part of the motivation for us to implement the calibration routines in question was to help with some issues discovered on two of our boards. We have ten boards in total, seven of which are passing all memory tests and do not show any signs of issues, one which is untested and two which have failing memory-tests during cold-boot. The two boards in question do function properly after pushing the reset-button, at which point they show no sign of memory-issues what so ever, even when stress-testing (using a run-time memory testing suite within our test application).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Aug 2016 07:50:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589691#M5677</guid>
      <dc:creator>tfe</dc:creator>
      <dc:date>2016-08-01T07:50:35Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589692#M5678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Let's consider&amp;nbsp; section 10.1.6.16.1 (Detailed Software Leveling Procedure) of the Vybrid RM :&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;To run leveling mode operations, the MMDC and PHY should be initialized, and the&lt;/P&gt;&lt;P&gt;appropriate delay parameters should be written with the value of delay that is needed for&lt;/P&gt;&lt;P&gt;each data slice X in the PHY. The delay parameters used by the software leveling option&lt;/P&gt;&lt;P&gt;are:&lt;/P&gt;&lt;P&gt;• Write Leveling: WRLVL_DLL_X bits&lt;/P&gt;&lt;P&gt;• Gate Training: RDLVL_GTDL_X bits&lt;/P&gt;&lt;P&gt;• Read Leveling: WRLVL_DL_X bits&lt;/P&gt;&lt;P&gt;At this point, the software should set the CR93[SWLVL_LOAD] to ’b1. This action will&lt;/P&gt;&lt;P&gt;trigger the MC to de-assert the CR94[SWLVL_OP_DONE]and the MC will initiate a&lt;/P&gt;&lt;P&gt;loading of the delay values into the data slices. The MC will then wait for the load&lt;/P&gt;&lt;P&gt;operation to complete, and initiate a write level strobe or a read burst. The MC will wait&lt;/P&gt;&lt;P&gt;for the response from the memory and save the response into the&lt;/P&gt;&lt;P&gt;CR94[SWLVL_RESP_2], CR95[SWLVL_RESP_1],CR94[SWLVL_RESP_0] for each&lt;/P&gt;&lt;P&gt;slice X. Once all responses are saved, the MC will assert the CR94[SWLVL_OP_DONE]&lt;/P&gt;&lt;P&gt;and generate an interrupt. This informs the user that the response data is available for the&lt;/P&gt;&lt;P&gt;initial delay values.&lt;/P&gt;&lt;P&gt;The software should use the response values CR94[SWLVL_RESP_2],&lt;/P&gt;&lt;P&gt;CR95[SWLVL_RESP_1],CR94[SWLVL_RESP_0] to determine the next operation. For&lt;/P&gt;&lt;P&gt;MC Evaluation mode, the response will indicate if the delay is appropriate, or must be&lt;/P&gt;&lt;P&gt;increased or decreased. If the delay must be changed, the new delay value should be&lt;/P&gt;&lt;P&gt;written to the associated parameter and the load sequence should be performed again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Is it possible to look at log of testing procedure&amp;nbsp; for this case : what values are loaded to the registers,&lt;/P&gt;&lt;P&gt;what are responses ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 08:52:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589692#M5678</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-08-09T08:52:51Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589693#M5679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our leveling procedures are based on the procedures described in the Reference Manual, including the section you are referring to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are the logs you asked for:&lt;/P&gt;&lt;P&gt;&lt;A href="http://pastebin.com/0xc21gFD" title="http://pastebin.com/0xc21gFD"&gt;Vybrid DDR3 Write leveling Log - Pastebin.com&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="http://pastebin.com/etEqbqfP" title="http://pastebin.com/etEqbqfP"&gt;Vybrid DDR3 Gate Training Log - Pastebin.com&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="http://pastebin.com/WAgUT94Z" title="http://pastebin.com/WAgUT94Z"&gt;Vybrid DDR3 Read Leveling Log - Pastebin.com&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each calibration is run after a forced ZQ-calibration. The top two lines state the ZQ PU- and PD-legs respectively.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A few observations:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Our boot-time DRAM-tests fail after the failed Gate Training and Read Leveling, but NOT after the failed Write Leveling.&lt;/LI&gt;&lt;LI&gt;The Gate Training is able to obtain a calibration value for one data-slice, but not for the other slice.&lt;/LI&gt;&lt;LI&gt;The Read and Write Leveling procedures are not able to obtain calibration values.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Aug 2016 10:36:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589693#M5679</guid>
      <dc:creator>tfe</dc:creator>
      <dc:date>2016-08-12T10:36:27Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589694#M5680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; thanks for the data. Note :the fact, that leveling calibration procedures &lt;/P&gt;&lt;P&gt;cannot obtain values may mean some inaccuracy in PCB design : please check DRAM&lt;/P&gt;&lt;P&gt;trace lengthes - if they meet recommended rules. &lt;/P&gt;&lt;P&gt;&amp;nbsp; Also, are prime data bits (DQ0/8) are connected properly ?&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Aug 2016 10:03:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589694#M5680</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-08-22T10:03:33Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589695#M5681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We will look into this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the mean time: Do you have any comments to the logs I sent you?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Aug 2016 10:09:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589695#M5681</guid>
      <dc:creator>tfe</dc:creator>
      <dc:date>2016-08-22T10:09:02Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589696#M5682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our HW engineer is ensuring us that the D0/8 is connected properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the trace lengths:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Net | Total Etch Length (mm)&lt;/P&gt;&lt;P&gt;DDR_A0 | 19.2536&lt;/P&gt;&lt;P&gt;DDR_A1 | 19.4868&lt;/P&gt;&lt;P&gt;DDR_A2 | 19.3504&lt;/P&gt;&lt;P&gt;DDR_A3 | 19.4200&lt;/P&gt;&lt;P&gt;DDR_A4 | 19.2596&lt;/P&gt;&lt;P&gt;DDR_A5 | 19.3363&lt;/P&gt;&lt;P&gt;DDR_A6 | 19.2846&lt;/P&gt;&lt;P&gt;DDR_A7 | 19.4457&lt;/P&gt;&lt;P&gt;DDR_A8 | 19.3298&lt;/P&gt;&lt;P&gt;DDR_A9 | 19.4759&lt;/P&gt;&lt;P&gt;DDR_A10 | 19.3770&lt;/P&gt;&lt;P&gt;DDR_A11 | 19.3899&lt;/P&gt;&lt;P&gt;DDR_A12 | 19.2149&lt;/P&gt;&lt;P&gt;DDR_A13 | 19.3452&lt;/P&gt;&lt;P&gt;DDR_A14 | 19.2646&lt;/P&gt;&lt;P&gt;DDR_BA0 | 19.4322&lt;/P&gt;&lt;P&gt;DDR_BA1 | 19.4387&lt;/P&gt;&lt;P&gt;DDR_BA2 | 19.4652&lt;/P&gt;&lt;P&gt;DDR_CASN | 19.5484&lt;/P&gt;&lt;P&gt;DDR_CKE0 | 20.5000&lt;/P&gt;&lt;P&gt;DDR_CLK0 | 24.7779&lt;/P&gt;&lt;P&gt;DDR_CLK0N | 24.8694&lt;/P&gt;&lt;P&gt;DDR_CS0N | 19.1552&lt;/P&gt;&lt;P&gt;DDR_DM0 | 23.8669&lt;/P&gt;&lt;P&gt;DDR_DM1 | 23.0069&lt;/P&gt;&lt;P&gt;DDR_DQS0 | 23.3302&lt;/P&gt;&lt;P&gt;DDR_DQS0N | 23.4173&lt;/P&gt;&lt;P&gt;DDR_DQS1 | 23.1457&lt;/P&gt;&lt;P&gt;DDR_DQS1N | 23.1168&lt;/P&gt;&lt;P&gt;DDR_D0 | 22.9372&lt;/P&gt;&lt;P&gt;DDR_D1 | 23.8522&lt;/P&gt;&lt;P&gt;DDR_D2 | 23.2087&lt;/P&gt;&lt;P&gt;DDR_D3 | 23.9195&lt;/P&gt;&lt;P&gt;DDR_D4 | 22.8930&lt;/P&gt;&lt;P&gt;DDR_D5 | 22.9457&lt;/P&gt;&lt;P&gt;DDR_D6 | 22.8074&lt;/P&gt;&lt;P&gt;DDR_D7 | 23.5879&lt;/P&gt;&lt;P&gt;DDR_D8 | 23.1138&lt;/P&gt;&lt;P&gt;DDR_D9 | 22.8126&lt;/P&gt;&lt;P&gt;DDR_D10 | 23.1966&lt;/P&gt;&lt;P&gt;DDR_D11 | 22.7116&lt;/P&gt;&lt;P&gt;DDR_D12 | 23.4505&lt;/P&gt;&lt;P&gt;DDR_D13 | 22.9836&lt;/P&gt;&lt;P&gt;DDR_D14 | 23.1454&lt;/P&gt;&lt;P&gt;DDR_D15 | 22.9478&lt;/P&gt;&lt;P&gt;DDR_ODT | 19.2805&lt;/P&gt;&lt;P&gt;DDR_RASN | 19.3943&lt;/P&gt;&lt;P&gt;DDR_RESETN | 16.8666&lt;/P&gt;&lt;P&gt;DDR_WEN | 19.2984&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Aug 2016 10:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589696#M5682</guid>
      <dc:creator>tfe</dc:creator>
      <dc:date>2016-08-22T10:46:52Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589697#M5683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;Generally DRAM signals traces meet recommendations.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to provide simulation of the signals on the board,&lt;/P&gt;&lt;P&gt;in order to take into account real design (say, vias) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Sep 2016 06:50:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589697#M5683</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-09-07T06:50:44Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589698#M5684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We did actually find an issue with the trace lengths, with the address lines being marginally too short. As such, we have created a separate thread on this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/824370"&gt;https://community.nxp.com/message/824370&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would like this thread to continue discussing the SW leveling features, described in the RM. As mentioned above, the RM does contain several inaccuracies, and therefore ask that you provide a complete and correct descriptions of this feature.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2016 06:39:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589698#M5684</guid>
      <dc:creator>tfe</dc:creator>
      <dc:date>2016-09-08T06:39:19Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589699#M5685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; as I know there are no plans to modify the RM, at least, &amp;nbsp;right now (because of &lt;BR /&gt;resources lack)&amp;nbsp;General recommendation from Mark Middleton : "[...]&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;if the customer &lt;BR /&gt;really wants to configure DDR3 in a Fly-By Topology, they can manually enter delay &lt;BR /&gt;values into the WRLVL_DL_0/1 fields based on trace length differences from their &lt;BR /&gt;layout. Mismatches up to 25% or tCK (clock period) are allowed, so the value in the &lt;BR /&gt;filed doesn’t have to be very accurate&lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2016 06:52:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589699#M5685</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-09-08T06:52:28Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589700#M5686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sorry if I was unclear in my previous post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please understand that we need a complete and correct description of the SW leveling procedure containing descriptions of edge-cases. As mentioned earlier, the procedure described in the RM is inaccurate and contains several mistakes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In particular, we need an answer to the following questions:&lt;/P&gt;&lt;P&gt;* How do we handle cases where the calculated delay values reach maximum/minimum? In the case of write leveling, the write level delay cycles = WRLVL_CLKDL + 0.5 x SW_HALF_CYCLE_SHIFT + WLLVK_DL_&amp;lt;X&amp;gt;/128 (from RM:p1498 - typo?), so we assume WRLVL_CLKDL can be adjusted if min/max is reached. Does read leveling and gate training have similar options?&lt;/P&gt;&lt;P&gt;* Generally what should we handle instances where no values are found? What adjustments should be made for the leveling procedures to be able to fund values?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are also aware of the DRAM Calibration Tool mentioned in the thread you are referring to. This SW is not an option to us, but were are insterested in a detailed description of the calibration procedure used. Is this something you can share with us?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2016 13:33:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589700#M5686</guid>
      <dc:creator>tfe</dc:creator>
      <dc:date>2016-09-08T13:33:13Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589701#M5687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/karinavalencia"&gt;karinavalencia&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can we expect a response on this soon?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2016 11:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589701#M5687</guid>
      <dc:creator>tfe</dc:creator>
      <dc:date>2016-09-20T11:55:08Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589702#M5688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/Yuri"&gt;Yuri&lt;/A&gt;‌ please continue with the follow up&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2016 13:00:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589702#M5688</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2016-09-20T13:00:53Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid DDR3 write leveling</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589703#M5689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; To get reprocessed, detailed description of SW leveling procedure, may be &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;as special app note, with corresponding SW tool, helping in this - some &lt;BR /&gt;additional resources should be involved here. Please escalate your request to &lt;BR /&gt;the marketing.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 06:09:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-DDR3-write-leveling/m-p/589703#M5689</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-09-21T06:09:16Z</dc:date>
    </item>
  </channel>
</rss>