<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックSDHC layout recommendations</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/514959#M5560</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing&amp;nbsp; Board&amp;nbsp; with Vybrid VF6 and I have doubt about SDHC layout recommentaions appears in paragraph 3.3.2.3 SD Card interface requirements of ref. doc. VYBRIDHDUG_HW_UserGuide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this paragrap appears:&lt;/P&gt;&lt;P&gt;1. The clock trace should be longer than the longest trace in the Data /Command group (+5mils).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is 5mils minimun distance or&amp;nbsp; maximum&amp;nbsp; ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. SD card interface layout requirements are very similar to those for the DDR one (see Section 3.5,&lt;/P&gt;&lt;P&gt;“DDR routing rules”).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;But in this section appears DDR3 recommnedations?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to kown routing recomentadion to SDHC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can somebody help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Jun 2016 11:49:36 GMT</pubDate>
    <dc:creator>fernandoalcaide</dc:creator>
    <dc:date>2016-06-06T11:49:36Z</dc:date>
    <item>
      <title>SDHC layout recommendations</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/514959#M5560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing&amp;nbsp; Board&amp;nbsp; with Vybrid VF6 and I have doubt about SDHC layout recommentaions appears in paragraph 3.3.2.3 SD Card interface requirements of ref. doc. VYBRIDHDUG_HW_UserGuide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this paragrap appears:&lt;/P&gt;&lt;P&gt;1. The clock trace should be longer than the longest trace in the Data /Command group (+5mils).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is 5mils minimun distance or&amp;nbsp; maximum&amp;nbsp; ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. SD card interface layout requirements are very similar to those for the DDR one (see Section 3.5,&lt;/P&gt;&lt;P&gt;“DDR routing rules”).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;But in this section appears DDR3 recommnedations?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to kown routing recomentadion to SDHC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can somebody help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jun 2016 11:49:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/514959#M5560</guid>
      <dc:creator>fernandoalcaide</dc:creator>
      <dc:date>2016-06-06T11:49:36Z</dc:date>
    </item>
    <item>
      <title>Re: SDHC layout recommendations</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/514960#M5561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Karina valencia Aguilar,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Can the NXP Vybrid Hardware team please comment on this?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jun 2016 05:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/514960#M5561</guid>
      <dc:creator>timesyssupport</dc:creator>
      <dc:date>2016-06-08T05:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: SDHC layout recommendations</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/514961#M5562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jiri-b36968"&gt;jiri-b36968&lt;/A&gt;​ can you comment please?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jun 2016 13:22:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/514961#M5562</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2016-06-08T13:22:58Z</dc:date>
    </item>
    <item>
      <title>Re: SDHC layout recommendations</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/514962#M5563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fernando,&lt;/P&gt;&lt;P&gt;yes, reference design uses DRAM memory type DDR3 (DDR is imprecise expression).&lt;/P&gt;&lt;P&gt;SDHC runs up to 50MHz.&lt;/P&gt;&lt;P&gt;- try to make lines short&lt;/P&gt;&lt;P&gt;- match all lines length.&lt;/P&gt;&lt;P&gt;- Add 5 mils to clk.&lt;/P&gt;&lt;P&gt;- try to keep lines on one layer.&lt;/P&gt;&lt;P&gt;- Ensure correct return path (continuous ground under lines)&lt;/P&gt;&lt;P&gt;- consider ESD protection if SD card is accessible to users.&lt;/P&gt;&lt;P&gt;/Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jun 2016 06:53:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/514962#M5563</guid>
      <dc:creator>jiri-b36968</dc:creator>
      <dc:date>2016-06-09T06:53:45Z</dc:date>
    </item>
    <item>
      <title>Re: SDHC layout recommendations</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/514963#M5564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jun 2016 11:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/514963#M5564</guid>
      <dc:creator>fernandoalcaide</dc:creator>
      <dc:date>2016-06-09T11:33:50Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/1138846#M6159</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 19:10:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/SDHC-layout-recommendations/m-p/1138846#M6159</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T19:10:47Z</dc:date>
    </item>
  </channel>
</rss>