<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Configuring CKO1 output PLL5 in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Configuring-CKO1-output-PLL5/m-p/510154#M5486</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I started with Yocto Jethro, and I successfully built a system image with the new 4.1 kernel.&lt;/P&gt;&lt;P&gt;I customized it with device tree, but I'm stuck with network. Our design use LAN8720 like Auto EVB, but RMII clock is provided by CKO1 output, CKO1(PTB10) is connected to RMII_CLKIN (PTA6) and connected to LAN8720 CLKIN (&lt;A _jive_internal="true" href="https://community.nxp.com/message/379224#comment-379224"&gt;see this&lt;/A&gt;). This design needs few BSP customizations and it worked fine with the old 3.0.15 kernel from Timesys.&lt;/P&gt;&lt;P&gt;PTB10 is well configured as CKO1 mode by device tree, and CCSOR, PLL5_CTRL configured by u-boot.&lt;/P&gt;&lt;P&gt;At the end of kernel init, just before rfs mount, RMII CLK stops, then eth0 becomes unavailable.&lt;/P&gt;&lt;P&gt;But I don't know if PTB10 iomux mode changed or CCSOR/PLL5_CTRL.&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Emmanuel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Mar 2016 12:27:58 GMT</pubDate>
    <dc:creator>Nouchi</dc:creator>
    <dc:date>2016-03-29T12:27:58Z</dc:date>
    <item>
      <title>Configuring CKO1 output PLL5</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Configuring-CKO1-output-PLL5/m-p/510154#M5486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I started with Yocto Jethro, and I successfully built a system image with the new 4.1 kernel.&lt;/P&gt;&lt;P&gt;I customized it with device tree, but I'm stuck with network. Our design use LAN8720 like Auto EVB, but RMII clock is provided by CKO1 output, CKO1(PTB10) is connected to RMII_CLKIN (PTA6) and connected to LAN8720 CLKIN (&lt;A _jive_internal="true" href="https://community.nxp.com/message/379224#comment-379224"&gt;see this&lt;/A&gt;). This design needs few BSP customizations and it worked fine with the old 3.0.15 kernel from Timesys.&lt;/P&gt;&lt;P&gt;PTB10 is well configured as CKO1 mode by device tree, and CCSOR, PLL5_CTRL configured by u-boot.&lt;/P&gt;&lt;P&gt;At the end of kernel init, just before rfs mount, RMII CLK stops, then eth0 becomes unavailable.&lt;/P&gt;&lt;P&gt;But I don't know if PTB10 iomux mode changed or CCSOR/PLL5_CTRL.&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Emmanuel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Mar 2016 12:27:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Configuring-CKO1-output-PLL5/m-p/510154#M5486</guid>
      <dc:creator>Nouchi</dc:creator>
      <dc:date>2016-03-29T12:27:58Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring CKO1 output PLL5</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Configuring-CKO1-output-PLL5/m-p/510155#M5487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt;​ can you help to attend this case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Apr 2016 21:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Configuring-CKO1-output-PLL5/m-p/510155#M5487</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2016-04-01T21:04:02Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring CKO1 output PLL5</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Configuring-CKO1-output-PLL5/m-p/510156#M5488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Emmanuel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We recently worked with this on different Vybrid hardware with the 4.1 kernel. I have attached several patches - one to setup CKO1 with ENET_CLK (you will need to add the 'enet-ref-clock-cko1' property to your device tree or remove this check in the patch), and another that cleans up pinmux settings for the LAN8720 PHY. Let me know if this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Apr 2016 22:25:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Configuring-CKO1-output-PLL5/m-p/510156#M5488</guid>
      <dc:creator>timesyssupport</dc:creator>
      <dc:date>2016-04-04T22:25:01Z</dc:date>
    </item>
  </channel>
</rss>