<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックHigh-level input higher than ovdd</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/High-level-input-higher-than-ovdd/m-p/495447#M5382</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir or Madam:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f3864;"&gt;we are evaluating multiple options to power the Vybrid using a single 3.3V supply. We are looking into a 1.5V-controlled LDO as the sequencing device shown in the block diagram attached. However, we have some concerns about the Vybrid. Could you please comment on our questions below?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;&lt;SPAN style="color: #1f3864;"&gt;We realize that there will be a little dropout voltage between 3.3V_P and 3.3V_S anyway. In our application, 3.3V_S will power the&amp;nbsp; Vybrid and 3.3V_P will power some peripheral digital electronics around it. It is possible that a logic-high input (powered by 3.3V_P) is higher than 3.3V_S that powers the Vybrid GPIO. The data sheet says that the high-level input has a max. value of ovdd, which is 3.3V_S in our case. Will a “higher-than-3.3V_S” cause any damage or malfunctions? What do you think?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f3864;"&gt;In the configuration shown in the block diagram, peripheral electronics will be powered on before the Vybrid (3.3V_P turns on before 3.3V_S). In case there are high-level inputs at some GPIO pins before 3.3V_S is on, we guess these inputs will be shunted to the internal 3.3V rail by the internal protection Schottky diodes. If this is true, the Vybrid 3.3V rail is virtually powered by the high-level input minus the voltage drop on the Schottky diodes. Will this phenomenon cause the Vybrid to enter a “partially-powered” state and malfunction?&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f3864;"&gt;Please kindly let us know what you think.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f3864;"&gt;Thanks and regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f3864;"&gt;Shoumin &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Feb 2016 23:16:48 GMT</pubDate>
    <dc:creator>shouminliu</dc:creator>
    <dc:date>2016-02-08T23:16:48Z</dc:date>
    <item>
      <title>High-level input higher than ovdd</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/High-level-input-higher-than-ovdd/m-p/495447#M5382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir or Madam:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f3864;"&gt;we are evaluating multiple options to power the Vybrid using a single 3.3V supply. We are looking into a 1.5V-controlled LDO as the sequencing device shown in the block diagram attached. However, we have some concerns about the Vybrid. Could you please comment on our questions below?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;&lt;SPAN style="color: #1f3864;"&gt;We realize that there will be a little dropout voltage between 3.3V_P and 3.3V_S anyway. In our application, 3.3V_S will power the&amp;nbsp; Vybrid and 3.3V_P will power some peripheral digital electronics around it. It is possible that a logic-high input (powered by 3.3V_P) is higher than 3.3V_S that powers the Vybrid GPIO. The data sheet says that the high-level input has a max. value of ovdd, which is 3.3V_S in our case. Will a “higher-than-3.3V_S” cause any damage or malfunctions? What do you think?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f3864;"&gt;In the configuration shown in the block diagram, peripheral electronics will be powered on before the Vybrid (3.3V_P turns on before 3.3V_S). In case there are high-level inputs at some GPIO pins before 3.3V_S is on, we guess these inputs will be shunted to the internal 3.3V rail by the internal protection Schottky diodes. If this is true, the Vybrid 3.3V rail is virtually powered by the high-level input minus the voltage drop on the Schottky diodes. Will this phenomenon cause the Vybrid to enter a “partially-powered” state and malfunction?&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f3864;"&gt;Please kindly let us know what you think.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f3864;"&gt;Thanks and regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f3864;"&gt;Shoumin &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Feb 2016 23:16:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/High-level-input-higher-than-ovdd/m-p/495447#M5382</guid>
      <dc:creator>shouminliu</dc:creator>
      <dc:date>2016-02-08T23:16:48Z</dc:date>
    </item>
    <item>
      <title>Re: High-level input higher than ovdd</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/High-level-input-higher-than-ovdd/m-p/495448#M5383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. Will a “higher-than-3.3V_S” cause any damage or malfunctions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. Yes, it can cause an excessive input current and even I/O buffer damage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q. Will this phenomenon cause the Vybrid to enter a “partially-powered” state and malfunction?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. Yes, this can cause a malfunction. The general requirement is that no I/O pins must be externally driven until the processor is powered on.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Feb 2016 05:47:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/High-level-input-higher-than-ovdd/m-p/495448#M5383</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-02-16T05:47:26Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/High-level-input-higher-than-ovdd/m-p/1138583#M6146</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 18:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/High-level-input-higher-than-ovdd/m-p/1138583#M6146</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T18:53:06Z</dc:date>
    </item>
  </channel>
</rss>