<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Motor Control using M4 in Vybrid in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Motor-Control-using-M4-in-Vybrid/m-p/493057#M5370</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no special support for this. I don't know much about Kinetises or about motor control but if there are peripherals on Vybrid which you need for motor control (PWMs?) and if you have some motor control code for another Cortex M4, then it's very likely that you can port the code to Vybrid easily.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Rene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Apr 2016 11:39:49 GMT</pubDate>
    <dc:creator>rendy</dc:creator>
    <dc:date>2016-04-14T11:39:49Z</dc:date>
    <item>
      <title>Motor Control using M4 in Vybrid</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Motor-Control-using-M4-in-Vybrid/m-p/493056#M5369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any software support available for motor control using Vybrid Cortex M4, seems there is motor control support in Kinetics V series (that have Cortex M4), can it be used with Vybrid M4 too?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;afzal &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Apr 2016 17:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Motor-Control-using-M4-in-Vybrid/m-p/493056#M5369</guid>
      <dc:creator>afzalmohammed</dc:creator>
      <dc:date>2016-04-09T17:49:35Z</dc:date>
    </item>
    <item>
      <title>Re: Motor Control using M4 in Vybrid</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Motor-Control-using-M4-in-Vybrid/m-p/493057#M5370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no special support for this. I don't know much about Kinetises or about motor control but if there are peripherals on Vybrid which you need for motor control (PWMs?) and if you have some motor control code for another Cortex M4, then it's very likely that you can port the code to Vybrid easily.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Rene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Apr 2016 11:39:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Motor-Control-using-M4-in-Vybrid/m-p/493057#M5370</guid>
      <dc:creator>rendy</dc:creator>
      <dc:date>2016-04-14T11:39:49Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Motor-Control-using-M4-in-Vybrid/m-p/1138551#M6144</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 18:50:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Motor-Control-using-M4-in-Vybrid/m-p/1138551#M6144</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T18:50:59Z</dc:date>
    </item>
  </channel>
</rss>