<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Does Vybrid MQX support include A5 core? in Vybrid Processors</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485453#M5251</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I did see this brochure. My question probably should have been, "Is anyone in the community running MQX on the Vybrid A5 core using the standard IDE tools provided by NXP?"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Mar 2016 17:31:08 GMT</pubDate>
    <dc:creator>kstolp</dc:creator>
    <dc:date>2016-03-17T17:31:08Z</dc:date>
    <item>
      <title>Does Vybrid MQX support include A5 core?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485451#M5249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does Vybrid MQX support only apply to the M4 core, or does it also apply to the A5 core?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Mar 2016 14:34:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485451#M5249</guid>
      <dc:creator>kstolp</dc:creator>
      <dc:date>2016-03-17T14:34:56Z</dc:date>
    </item>
    <item>
      <title>Re: Does Vybrid MQX support include A5 core?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485452#M5250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It does support the A5 core, please take a look at the following document for a detailed version list and their support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/soft_dev_tools/doc/fact_sheet/MQXFS.pdf" title="http://cache.nxp.com/files/soft_dev_tools/doc/fact_sheet/MQXFS.pdf"&gt;http://cache.nxp.com/files/soft_dev_tools/doc/fact_sheet/MQXFS.pdf&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Mar 2016 16:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485452#M5250</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2016-03-17T16:31:33Z</dc:date>
    </item>
    <item>
      <title>Re: Does Vybrid MQX support include A5 core?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485453#M5251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I did see this brochure. My question probably should have been, "Is anyone in the community running MQX on the Vybrid A5 core using the standard IDE tools provided by NXP?"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Mar 2016 17:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485453#M5251</guid>
      <dc:creator>kstolp</dc:creator>
      <dc:date>2016-03-17T17:31:08Z</dc:date>
    </item>
    <item>
      <title>Re: Does Vybrid MQX support include A5 core?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485454#M5252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/SergioSolis"&gt;SergioSolis&lt;/A&gt;​ are you able to continue with the follow up?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Mar 2016 21:48:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485454#M5252</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2016-03-17T21:48:14Z</dc:date>
    </item>
    <item>
      <title>Re: Does Vybrid MQX support include A5 core?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485455#M5253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, I haven't&amp;nbsp; run MQX in the Vybrid A5.. &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/alejandrolozano"&gt;alejandrolozano&lt;/A&gt;​ you have more experience with MQX, have you used the A5 with MQX?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Mar 2016 15:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485455#M5253</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2016-03-18T15:04:00Z</dc:date>
    </item>
    <item>
      <title>Re: Does Vybrid MQX support include A5 core?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485456#M5254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, theres support in MQX for the CA5. There very basic examples found in the&amp;lt; MQX_INSTALLATION_FOLDER&amp;gt;/mqx/examples/ That you can use as reference. There are multiple exmaples working in IAR, DS-5 or even using Makefiles with the command line. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you having some kind of problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Mar 2016 18:25:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485456#M5254</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2016-03-28T18:25:36Z</dc:date>
    </item>
    <item>
      <title>Re: Does Vybrid MQX support include A5 core?</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485457#M5255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the information. I don't have a specific problem with Vybrid. I am looking for a processor that can do data transfers using UARTS, USB flash drive, and 10/100 Ethernet. All transfers are simultaneous. I'd like to have two UARTS running full duplex at 1Mbps and would like to write data to a USB flash drive at about 4 MB/sec, and send and receive data TCP/IP at about 2 MB/sec. I have been looking at Cortex M4/M7 MCU's, but I'm not sure they can keep up with these data rates. I've also been looking at the A9 processors. I think A9 can do the data rates, but they have more features than I really need. I think A9 is also more power hungry than I want. The Vybrid looks like it may be a good middle ground, but I think the A5 was intended to run Linux, and maybe the Vybrid A5 running Linux can meet my performance requirements, but if it can't I was thinking MQX running on the A5 might be a good fall back solution.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Mar 2016 13:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Does-Vybrid-MQX-support-include-A5-core/m-p/485457#M5255</guid>
      <dc:creator>kstolp</dc:creator>
      <dc:date>2016-03-31T13:40:27Z</dc:date>
    </item>
  </channel>
</rss>