<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: Vybrid Linux BSP Support for eMMC</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-Linux-BSP-Support-for-eMMC/m-p/479376#M5227</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andreas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While there is support for some eMMC devices in the 3.13 Linux kernel in the Timesys BSP, this support is not specifically enabled for the Vybrid platform. At a minimum, supporting this would require modifying the kernel configuration and device tree source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Feb 2016 16:07:20 GMT</pubDate>
    <dc:creator>timesyssupport</dc:creator>
    <dc:date>2016-02-01T16:07:20Z</dc:date>
    <item>
      <title>Vybrid Linux BSP Support for eMMC</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-Linux-BSP-Support-for-eMMC/m-p/479375#M5226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We wish to use eMMC with the Vybrid.Does the linux BSP(s) from &lt;A _jive_internal="true" data-containerid="-1" data-containertype="-1" data-objectid="214905" data-objecttype="3" href="https://community.nxp.com/people/timesyssupport"&gt;Timesys Support&lt;/A&gt; support eMMC memory technologies currently?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From different forum posts, it seems a bit unclear if this support is in place or not.&lt;/P&gt;&lt;P&gt;Please clarify.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MQX does not support this in their BSP;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/357992"&gt;Vybrid, eMMC, MQX&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TimeSys has commented a similar request at an earlier stage&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/357545"&gt;How to use both sdhc0 and sdhc1?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I.Mx Sabre Board with Linux seems to support this&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/324387"&gt;Booting Linux from eMMC&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Andreas Eknes Lie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Feb 2016 10:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-Linux-BSP-Support-for-eMMC/m-p/479375#M5226</guid>
      <dc:creator>almagest</dc:creator>
      <dc:date>2016-02-01T10:22:29Z</dc:date>
    </item>
    <item>
      <title>Re: Vybrid Linux BSP Support for eMMC</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-Linux-BSP-Support-for-eMMC/m-p/479376#M5227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andreas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While there is support for some eMMC devices in the 3.13 Linux kernel in the Timesys BSP, this support is not specifically enabled for the Vybrid platform. At a minimum, supporting this would require modifying the kernel configuration and device tree source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Feb 2016 16:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-Linux-BSP-Support-for-eMMC/m-p/479376#M5227</guid>
      <dc:creator>timesyssupport</dc:creator>
      <dc:date>2016-02-01T16:07:20Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-Linux-BSP-Support-for-eMMC/m-p/1138364#M6136</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 18:38:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Vybrid-Linux-BSP-Support-for-eMMC/m-p/1138364#M6136</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T18:38:20Z</dc:date>
    </item>
  </channel>
</rss>