<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: Java on Vybrid</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476344#M5189</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jaroslav,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While your Yocto build will not generate a Debian-based image, you can still change the kernel configuration and device tree source for the Vybrid kernel in this build. I would recommend creating a custom layer, where in this layer, you can override the kernel defconfig to change the kernel configuration, and add a patch to the kernel source (or change the kernel source URI altogether), in order to change the device tree source. Here is some more information about creating a custom layer for your Yocto build:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.yoctoproject.org/docs/1.8/bsp-guide/bsp-guide.html#creating-a-new-bsp-layer-using-the-yocto-bsp-script" title="http://www.yoctoproject.org/docs/1.8/bsp-guide/bsp-guide.html#creating-a-new-bsp-layer-using-the-yocto-bsp-script"&gt;Yocto Project Board Support Package Developer's Guide&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As Sanchayan said, you can download and include the meta-java layer in your Yocto build. The meta-java layer can provide numerous Java utilities for your build, including the JamVM JVM. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Jan 2016 19:31:32 GMT</pubDate>
    <dc:creator>timesyssupport</dc:creator>
    <dc:date>2016-01-18T19:31:32Z</dc:date>
    <item>
      <title>Java on Vybrid</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476339#M5184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is it possible to run java application on Vybrid?&lt;/P&gt;&lt;P&gt;Do I can use JVM for ARM?&lt;/P&gt;&lt;P&gt;If so, what I should to do to make it work?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jan 2016 10:21:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476339#M5184</guid>
      <dc:creator>cerma</dc:creator>
      <dc:date>2016-01-08T10:21:30Z</dc:date>
    </item>
    <item>
      <title>Re: Java on Vybrid</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476340#M5185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, Java can be used on the Vybrid. What exactly are you running on the Vybrid? Linux? Which distribution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, in case of Angstrom distribution with an OpenEmbedded build, java can be installed using the meta-java layer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Sanchayan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jan 2016 05:20:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476340#M5185</guid>
      <dc:creator>sanchayanmaity</dc:creator>
      <dc:date>2016-01-11T05:20:10Z</dc:date>
    </item>
    <item>
      <title>Re: Java on Vybrid</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476341#M5186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Currently I am trying get to work most recent version of yocto (1.8). It would be awesome if it would be more like arm (i.MX6) where I could download kernel code and change it as I like and than recompile. So far is yocto very confusing for me. So you could provide some manual and (or) something what would be similar to working with classic kernel &lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN class="hps"&gt;I would highly&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;appreciate it.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;My idea is as follows:&lt;/P&gt;&lt;P&gt;- run some Linux distribution (ideally Debian based) and be able to change kernel config and maybe DTS&lt;/P&gt;&lt;P&gt;- get JVM to work for user space apps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jan 2016 08:12:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476341#M5186</guid>
      <dc:creator>cerma</dc:creator>
      <dc:date>2016-01-11T08:12:39Z</dc:date>
    </item>
    <item>
      <title>Re: Java on Vybrid</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476342#M5187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May be the following article on our Blog will be of help&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.toradex.com/blog/the-yocto-projects-reference-distribution-poky-on-toradex-hardware" title="https://www.toradex.com/blog/the-yocto-projects-reference-distribution-poky-on-toradex-hardware"&gt;https://www.toradex.com/blog/the-yocto-projects-reference-distribution-poky-on-toradex-hardware&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have your own hardware or are you using Vybrid Tower platform? The meta-fsl-arm layer has the MACHINE &lt;A href="http://git.yoctoproject.org/cgit/cgit.cgi/meta-fsl-arm/tree/conf/machine/twr-vf65gs10.conf?h=master" style="color: #005580; text-decoration: underline; font-family: 'Helvetica Neue', Helvetica, Arial, sans-serif;"&gt;twr-vf65gs10&lt;/A&gt; for building for Tower boards.&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.yoctoproject.org/cgit/cgit.cgi/meta-fsl-arm/tree/conf/machine/twr-vf65gs10.conf?h=master" title="http://git.yoctoproject.org/cgit/cgit.cgi/meta-fsl-arm/tree/conf/machine/twr-vf65gs10.conf?h=master"&gt;meta-fsl-arm - Layer containing Freescale ARM hardware support metadata&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It uses the 4.1 kernel&lt;/P&gt;&lt;P&gt;&lt;A href="http://layers.openembedded.org/layerindex/recipe/5886/" title="http://layers.openembedded.org/layerindex/recipe/5886/"&gt;OpenEmbedded Metadata Index - linux-fslc&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can in fact download a mainline kernel even and use it. You would need a Yocto build with the meta-java layer added for adding java to the image build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Sanchayan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jan 2016 10:03:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476342#M5187</guid>
      <dc:creator>sanchayanmaity</dc:creator>
      <dc:date>2016-01-11T10:03:51Z</dc:date>
    </item>
    <item>
      <title>Re: Java on Vybrid</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476343#M5188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/timesyssupport"&gt;timesyssupport&lt;/A&gt;​ can you share your comments here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 18:39:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476343#M5188</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2016-01-18T18:39:43Z</dc:date>
    </item>
    <item>
      <title>Re: Java on Vybrid</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476344#M5189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jaroslav,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While your Yocto build will not generate a Debian-based image, you can still change the kernel configuration and device tree source for the Vybrid kernel in this build. I would recommend creating a custom layer, where in this layer, you can override the kernel defconfig to change the kernel configuration, and add a patch to the kernel source (or change the kernel source URI altogether), in order to change the device tree source. Here is some more information about creating a custom layer for your Yocto build:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.yoctoproject.org/docs/1.8/bsp-guide/bsp-guide.html#creating-a-new-bsp-layer-using-the-yocto-bsp-script" title="http://www.yoctoproject.org/docs/1.8/bsp-guide/bsp-guide.html#creating-a-new-bsp-layer-using-the-yocto-bsp-script"&gt;Yocto Project Board Support Package Developer's Guide&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As Sanchayan said, you can download and include the meta-java layer in your Yocto build. The meta-java layer can provide numerous Java utilities for your build, including the JamVM JVM. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timesys Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 19:31:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/476344#M5189</guid>
      <dc:creator>timesyssupport</dc:creator>
      <dc:date>2016-01-18T19:31:32Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/1138329#M6133</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 18:36:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/Java-on-Vybrid/m-p/1138329#M6133</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T18:36:08Z</dc:date>
    </item>
  </channel>
</rss>