<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックBSDL File for VF5xxR</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/BSDL-File-for-VF5xxR/m-p/473475#M5178</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;@Richard Stulens​&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi Richard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the Cascon tool from Göpel electronic I can program an external EEProm (M95256WMN6).&lt;/P&gt;&lt;P&gt;But it seems, that the BSDL File which I found ("Vybrid F Series 364MAPBGA BSDL Silicon Revision 1.1") is does not to 100% compatible to the VF5xxR Controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--------------------------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;I urgently need a BSDL file because an EEProm should to be programmed via the S&lt;STRONG&gt;VF5&lt;/STRONG&gt;12&lt;STRONG&gt;R&lt;/STRONG&gt;3K1CMK4 (VF5xxR) controller.&lt;/P&gt;&lt;P&gt;See also my question &lt;A _jive_internal="true" data-containerid="11048" data-containertype="14" data-content-finding="Community" data-objectid="390606" data-objecttype="1" href="https://community.nxp.com/thread/390606"&gt;Chip doesn't seem to work correctly with this BSDL files "Vybrid F Series 364MAPBGA BSDL Silicon Revision 1.1 (REV 0) " or "bga_364_v2.bsdl"&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;--------------------------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Can you help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Andreas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Apr 2016 15:34:39 GMT</pubDate>
    <dc:creator>andreas_veges</dc:creator>
    <dc:date>2016-04-25T15:34:39Z</dc:date>
    <item>
      <title>BSDL File for VF5xxR</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/BSDL-File-for-VF5xxR/m-p/473475#M5178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;@Richard Stulens​&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi Richard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the Cascon tool from Göpel electronic I can program an external EEProm (M95256WMN6).&lt;/P&gt;&lt;P&gt;But it seems, that the BSDL File which I found ("Vybrid F Series 364MAPBGA BSDL Silicon Revision 1.1") is does not to 100% compatible to the VF5xxR Controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--------------------------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;I urgently need a BSDL file because an EEProm should to be programmed via the S&lt;STRONG&gt;VF5&lt;/STRONG&gt;12&lt;STRONG&gt;R&lt;/STRONG&gt;3K1CMK4 (VF5xxR) controller.&lt;/P&gt;&lt;P&gt;See also my question &lt;A _jive_internal="true" data-containerid="11048" data-containertype="14" data-content-finding="Community" data-objectid="390606" data-objecttype="1" href="https://community.nxp.com/thread/390606"&gt;Chip doesn't seem to work correctly with this BSDL files "Vybrid F Series 364MAPBGA BSDL Silicon Revision 1.1 (REV 0) " or "bga_364_v2.bsdl"&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;--------------------------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Can you help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Andreas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Apr 2016 15:34:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/BSDL-File-for-VF5xxR/m-p/473475#M5178</guid>
      <dc:creator>andreas_veges</dc:creator>
      <dc:date>2016-04-25T15:34:39Z</dc:date>
    </item>
    <item>
      <title>Re: BSDL File for VF5xxR</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/BSDL-File-for-VF5xxR/m-p/473476#M5179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/richard_stulens"&gt;richard_stulens&lt;/A&gt;​ FYI&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Apr 2016 17:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/BSDL-File-for-VF5xxR/m-p/473476#M5179</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2016-04-25T17:22:04Z</dc:date>
    </item>
    <item>
      <title>Re: BSDL File for VF5xxR</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/BSDL-File-for-VF5xxR/m-p/473477#M5180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/andreas.veges@rafi.de"&gt;andreas.veges@rafi.de&lt;/A&gt;​ is this case same&amp;nbsp;&amp;nbsp; as&amp;nbsp; &lt;A href="https://community.nxp.com/thread/390606"&gt;Chip doesn't seem to work correctly with this BSDL files "Vybrid F Series 364MAPBGA BSDL Silicon Revision 1.1 (REV 0) " …&lt;/A&gt;&amp;nbsp; ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 May 2016 18:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/BSDL-File-for-VF5xxR/m-p/473477#M5180</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2016-05-02T18:16:01Z</dc:date>
    </item>
    <item>
      <title>Re: BSDL File for VF5xxR</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/BSDL-File-for-VF5xxR/m-p/473478#M5181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/karinavalencia"&gt;karinavalencia&lt;/A&gt;​ Yes. You can delete it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2016 06:51:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/BSDL-File-for-VF5xxR/m-p/473478#M5181</guid>
      <dc:creator>andreas_veges</dc:creator>
      <dc:date>2016-05-03T06:51:47Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/BSDL-File-for-VF5xxR/m-p/1138286#M6131</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 18:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/BSDL-File-for-VF5xxR/m-p/1138286#M6131</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T18:33:20Z</dc:date>
    </item>
  </channel>
</rss>