<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Vybrid ProcessorsのトピックRe: NAND firmware compilation</title>
    <link>https://community.nxp.com/t5/Vybrid-Processors/NAND-firmware-compilation/m-p/438548#M4875</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Great, that looks promising. Thank you, Alejandro.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Aug 2015 06:12:58 GMT</pubDate>
    <dc:creator>kubiznak_petr</dc:creator>
    <dc:date>2015-08-25T06:12:58Z</dc:date>
    <item>
      <title>NAND firmware compilation</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/NAND-firmware-compilation/m-p/438544#M4871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any available reference software (MQX or bare board), showing how to compile it for booting from NAND FLASH? The MfgTool for Vybrid features led_sample.bin, which executes well, but I'm not able to compile any custom SW which would run. I explored the Image Vector Table (IVT) of multiple Vybrid A5 MQX programs, compiled under IAR for both IntRam and DDR configurations, and they are all totally different from the expected format, described in chapter 19.6 of the Vybrid Reference Manual, Rev. 7, 06/2014. I tried to modify the .icf file, but without success. (ICF file format description might be useful.)&lt;/P&gt;&lt;P&gt;Just to be clear - I'm able to upload u-boot via MfgTool and flash the binary into the NAND flash, but I'm not able to compile working custom firmware binary.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 12:30:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/NAND-firmware-compilation/m-p/438544#M4871</guid>
      <dc:creator>kubiznak_petr</dc:creator>
      <dc:date>2015-08-13T12:30:39Z</dc:date>
    </item>
    <item>
      <title>Re: NAND firmware compilation</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/NAND-firmware-compilation/m-p/438545#M4872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not tried that out yet. But after skimming through the sources and taking a look at the led binary sample I noticed the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The led binary you mention, contains the IVT already with the 0x400 offset. As far as I see the MQX binaries lack of the IVT, therefore you have to add the IVT with the offset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2015 16:48:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/NAND-firmware-compilation/m-p/438545#M4872</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-08-20T16:48:46Z</dc:date>
    </item>
    <item>
      <title>Re: NAND firmware compilation</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/NAND-firmware-compilation/m-p/438546#M4873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alejandro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply. I'm aware of the offset and some other required characteristics of the IVT. I don't know how to achieve it with an MQX app, though, nor I managed to build a bare board project that way, yet. Any reference source code would be pretty much of use.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2015 06:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/NAND-firmware-compilation/m-p/438546#M4873</guid>
      <dc:creator>kubiznak_petr</dc:creator>
      <dc:date>2015-08-24T06:18:19Z</dc:date>
    </item>
    <item>
      <title>Re: NAND firmware compilation</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/NAND-firmware-compilation/m-p/438547#M4874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;An example that may help as reference is the mqx\examples\bootloader_vybrid_qspixip.&lt;/P&gt;&lt;P&gt;That example contains an IVT and a QSPI flash configuration that you have to get rid of it.&lt;/P&gt;&lt;P&gt;That way you can just modify the IVT structure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2015 17:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/NAND-firmware-compilation/m-p/438547#M4874</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-08-24T17:31:30Z</dc:date>
    </item>
    <item>
      <title>Re: NAND firmware compilation</title>
      <link>https://community.nxp.com/t5/Vybrid-Processors/NAND-firmware-compilation/m-p/438548#M4875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Great, that looks promising. Thank you, Alejandro.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Aug 2015 06:12:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Vybrid-Processors/NAND-firmware-compilation/m-p/438548#M4875</guid>
      <dc:creator>kubiznak_petr</dc:creator>
      <dc:date>2015-08-25T06:12:58Z</dc:date>
    </item>
  </channel>
</rss>